STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Nucleo L053 & IDB04A1 & IDB002V1

Posted on December 24, 2014 at 03:02We're looking to evaluate the Nucleo STM32L053 with the BlueNRG shield.  On hand, we also have the IDB002V1 eval kit for the BlueNRG.We're following the documentation in AN4559 to evaluate the SensorDemo program. ...

eleventen by Associate III
  • 1070 Views
  • 2 replies
  • 0 kudos

Which CubeMX packages should be installed?

Posted on January 26, 2015 at 23:25Are the cube firmware packages cumulative? Version STMCubeF4 1.4.0 came out recently, but I noticed that version 1.2.0 is significantly smaller than 1.1.0 or 1.3.0. This hints that all of the packages should be ins...

STM32L - can't change Brownout level

Posted on January 26, 2015 at 11:25 Hey there, today i wanted to change the brownout level from 1 to 4, but i failed. I'm using the STM32L151VDT6 and the following code at startup if ((FLASH_OB_GetBOR() & 0x0F) != OB_BOR_LEVEL...

juergen23 by Associate II
  • 2552 Views
  • 3 replies
  • 0 kudos

best way to use SWDIO and SWDCK

Posted on January 02, 2015 at 08:38Hi everybody, i'm working on a custom board and experiencing a strange problem: if the two cables of SWDIO and SWDCK (they go from a stm32f4 discovery board to my board) are close Keil doesn't recognize the cortex ...

nTRST with Debug+ETM connector on ULINK PRO

Posted on February 04, 2015 at 12:58I am using ULINK-PRO to debug a STM32F4.  I have connected the target as per the Cortex Debug+ETM 20 pin.  I have connected TRACE_D1 to nTRST as I believe these pins are multiplexed within the ULINK PRO.  i.e. nTR...

kb by Associate II
  • 1313 Views
  • 1 replies
  • 0 kudos

writing to a port which is not available

Posted on February 04, 2015 at 07:47 Hello, we have a small software (bootloader) running on a STM32F103. In a new project, we selecte a ''smaller'' type the STM32F105 with less pins. In the bootloader we set a push pull port high. On the new contro...

Writing and reading flash

Posted on February 04, 2015 at 14:06 hi i have an stm32f4 and i try to write and read flash value. #include < stm32f4xx_hal.h > #include < stm32f4xx.h > #include < stm32f4-hal /stm32f4xx_hal_flash.h> float dataflash1 = ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.