STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F205RB - unused pins

Posted on February 04, 2015 at 22:37 Hello - I have a few questions on unused pins for this device - We will not use the RTC.  Can we leave the LSE pins unconnected?  Or do we tie them to a rail?We will not use the ADC, DAC, sensors etc.  Can we l...

rick2399 by Associate II
  • 1862 Views
  • 3 replies
  • 0 kudos

STM429 LCD always scroll down

Posted on February 05, 2015 at 14:03I run STemWin helloworld demo in my own STM429 board which has a 7'' LCD.  It can display ''Hello world'', but screen always scrolls down. Is it the problem about HSYNC/VSYNC? How can I solve this problem. Please...

ray by Associate II
  • 810 Views
  • 1 replies
  • 0 kudos

STM429 LCD always vertically scroll down

Posted on February 05, 2015 at 14:50I run STemWin helloworld demo in my own STM429 board which has a 7'' LCD.  It can display ''Hello world'', but screen always scrolls down. Is it the problem about HSYNC/VSYNC? How can I solve this problem. Please...

ray by Associate II
  • 975 Views
  • 1 replies
  • 0 kudos

STM32F07xx: Behaviour if internal flash is corrupted

Posted on February 05, 2015 at 14:05Hi all, how does the STM32 behaves during a power-on start-up if the flash is corrupted? Does it enters the boot mode again to try the USB DFU again, do I have to reanimate with a debugger, ... ? This condition ma...

stm32f103 clock (RCC) problem

Posted on February 05, 2015 at 12:42Hi all,i'm working on 103 MCU. first step is to bring up the 72Mhz clock.problem is i'm able to get clock upto 64Mhz (tested with systick),but when i configure pll mul factor to 9 control is moving to default hand...

Start two timers synchronous in STM32F1 eval board

Posted on February 05, 2015 at 06:30Hello,I have to start two timers exactly at the same time... like In my program i am using TIM3 four channels for 4 four hall sensors and TIM4 for 5 hall sensor... I need to start all the 5 hall sensors at time.. ...

santhosh by Associate
  • 1226 Views
  • 1 replies
  • 0 kudos

STM32F2 and two nand targets

Posted on February 05, 2015 at 05:09Hi, I'm working on a board that interfaces an STM32F2 with a 4GB nand flash from Micron MT29F32G08AFABAWP:B. That nand flash is split up internally to two different dies. They use most of the same data and control...

Bug in STM32cube HID code for STM32F103

Posted on February 01, 2015 at 23:22I just started playing with the USB code for the stm32f103c8.  I found it quite impressive.  It was the only tool I tried so far that was able to produce working code for a HID device that enumerated properly.  Ho...

h500ca by Associate
  • 1136 Views
  • 1 replies
  • 0 kudos

Stm32 StdPeriph driver and Eclipse CDT configuration

Posted on February 04, 2015 at 22:57Hi guys! I have a problem with my stm32 discovery board. I installed eclipse, gnu arm plugin(version 2.2.1), gcc arm none eabi(4_9-2014q4).I did not install latest gnu arm plugin because i don't want to use hal_dr...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.