STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Sonar (HCSR04) on STM32F3-discovery

Posted on February 28, 2015 at 14:25  The original post was too long to process during our migration. Please click on the attachment to read the original post.

kahseng05 by Associate II
  • 1627 Views
  • 1 replies
  • 0 kudos

stm32F2 Max Speed Master SPI

Posted on February 28, 2015 at 10:47Hi. I'm trying to set the spi at max speed (in theory 30mbit/s spi in stm32F2), but I just get 15mbits on SPI output.This is my spi initialization (for SPI3). I'm using DMA to transfer a buffer, but in theory that...

pedro23 by Senior
  • 1033 Views
  • 1 replies
  • 0 kudos

CubeMX HAL_USART_Receive_IT returning always Noise Error

Posted on February 28, 2015 at 09:18 I have checked the demo in: STM32Cube_FW_F4_V1.3.0\Projects\STM32F4-Discovery\Examples\UART\UART_TwoBoards_ComIT I setup same configuration following STM32CubeMX and I can Tx but I can't Rx. Instead...

eperis by Associate
  • 693 Views
  • 0 replies
  • 0 kudos

SPI Interbyte delay

Posted on February 27, 2015 at 19:44Hi all,I'm doing some testing with STM32L151, and I'm trying to send a bulk of data over SPI.I'm using SPI in interrupt mode, my CPU is set to 32MHz, SPI is set to 16MHz.When I send a byte, I'm waiting for a SPI_I...

srdjan by Associate II
  • 2702 Views
  • 4 replies
  • 0 kudos

SPI3 RXNE SLOW

Posted on May 27, 2012 at 10:40Hi,I am using the STM32F107 micro, and tied an SD card into its SPI3 remmaped pins. As i saw in the datasheet the RXNE bit responce after the trasnmission is at worse 1 bit clock in duration. As you can see from the DS...

timos by Associate
  • 1347 Views
  • 3 replies
  • 0 kudos

Autosar mcal for STM32F4

Posted on February 27, 2015 at 17:54Hi, do ST provide an mcal layer for use with an Autosar OS on the STM32F4 range of micros? Thanks Andy

Problem with Systick Timer STM32F103RB

Posted on February 27, 2015 at 11:12Hello everybody, Im working on a project with a nucleo-F103RB with the IDE EM::Blocks and I have some issues with the Systick Timer. I read some relative post but none of them solve my problem. This is the way i c...

unidentified debug fault

Posted on February 27, 2015 at 05:59my application works perfectly in debug mode.as soon as i get disconnected from debug mode and tries to restart application by pressing reset button ,lcd goes white on stm32f429.i mean i dont know whats happening ...

kiran2 by Associate II
  • 1436 Views
  • 2 replies
  • 0 kudos

STM32F105VC Flash programming problem

Posted on February 26, 2015 at 05:00Hello. I created MODBUS firmware bootloader and it works good, but when I upload main firmware it does not program flash. Bootloader is compiled with base 0x08000000 and uploaded by JTAG. Then main firmware is com...

georg2 by Associate
  • 2077 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.