STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4: I2C with re-starts

Posted on February 27, 2015 at 11:58 Just wondering if it's possible to send/receive I2C data using re-starts instead of Stop/Start. So I transmit data with: if( HAL_I2C_Master_Transmit(&hi2c2, ADDR_DS, i2c_data, 5, 1000) == HAL_OK...

joe by Associate III
  • 797 Views
  • 0 replies
  • 0 kudos

STMF0 Timer DMA direct vs. DMAR register

Posted on February 27, 2015 at 10:21We are using TIM16 for pwm audio output. We want to make it more efficient by using DMA. The DMA triggering is done using TIM6 which controls the rate.I would use a direct access to TIM16 by configuring  DMA_Perip...

roy23 by Associate II
  • 714 Views
  • 0 replies
  • 0 kudos

lwip ping slow in debug mode

Posted on February 26, 2015 at 09:35I use cube1.3.0 lwip on STM429. It can work and ping ok in release mode. But in debug mode when I use keil and st-link, it always timeout. I have tried ping and TCP recv/send, it's response 2-3 seconds. Link bel...

ray by Associate II
  • 932 Views
  • 1 replies
  • 0 kudos

USART Interrupt Handler

Posted on February 26, 2015 at 18:51HI.I have a board with stm32f407. I Have ported UCOSII on it and in one of tasks enable USART3 and its interrupt handler. USART works correct at sending  but my probelm is this:I can not recieve any thing on my in...

STM32F4 timing application question

Posted on February 05, 2015 at 19:44The application is to use a STM32F4, but not allow the core to enter any level of ISR at the time it's supposed to service a TIMER interrupt. The application needs the TIMER events to be repeatable down to clock c...

STM32F4xx small size

Posted on February 25, 2015 at 00:53Hi,do you (ST) have in plan to make a small footprint STM32F4xx devices?Like 32 or 48 pins?There are times when you just need a lot of power (FFT, DSP) but not so much pins.Like STM32F446 is a great, but unfortuna...

tm3341 by Associate II
  • 1903 Views
  • 6 replies
  • 0 kudos

STM32F4 oddities in stm32f4xx_hal_adc.c

Posted on January 23, 2015 at 01:57 In the STM32F4xx HAL, file stm32f4xx_hal_adc.c there is this code /* Check if ADC peripheral is disabled in order to enable it and wait during Tstab time the ADC's stabilization */ if((hadc->In...

STM32F373 SDADC1 trigger by Timer 19

Posted on November 07, 2014 at 11:22 Hi all! This is my first project with ST micro. I have evaluation board stm32373c-eval. I have generated low level code with STM32cubeMX. I want start SDADC1 triggered by TIMER19 but the SDADC1 start...

enrico by Associate
  • 1292 Views
  • 1 replies
  • 0 kudos

STM32L053 I2C size managment error

Posted on November 04, 2014 at 17:13Hello everybody.I hope someone could help...I work with a STM32L053 and should communicate over I2C with a sensor. I checked the delivered examples from the STM32CubeL0 and can initialise the I2C. But when I send ...

thierry2 by Associate
  • 1214 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.