STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 General questions

Posted on March 30, 2015 at 11:26Hello, I try to make a demoboard with a STM32F4 controller but I have some problems: Which pins I need to use the stlink programmer from a nucleo board (swdio, swclk ,... )? I found in the datasheet, that some functi...

Timer Interrupt for 1ms

Posted on March 30, 2015 at 14:16I am using STM32F207 VG controller for my learning.I have few following doubts.I want to use timer for up counting.Timer clock is set to 36 MHz.I want to generate timer interrupt for every 1 ms.With what values i nee...

er by Associate II
  • 4756 Views
  • 5 replies
  • 0 kudos

Hardfault Cause on STM32F0xx?

Posted on March 31, 2015 at 13:57Hi, I have tried to find some information about registers signalling the cause of a hard fault  on an STM32F072 but couldn't find anything useful. If anyone could give me some directions I would be glad. Regards, Kil...

STM32F4 Discovery timer syncronization

Posted on March 30, 2015 at 16:46 I am currently trying to generate a squarewave on A8 with TIM1 (50% duty PWM1) and use TIM2 as a slave to trigger an interrupt every 4096th tick (this is used to reset the counter of an LED driver and to push ne...

Leonelf by Associate II
  • 2682 Views
  • 8 replies
  • 0 kudos

VREFINT magically turns on, MCU does not know about it

Posted on March 27, 2015 at 17:23 It would seem VREFINT magically turns on after coming out of sleep/stop even though it is not being used on the STM32L053 (nucleo board). It turns off for the first sleep/stop, then it wont turn off again. The M...

Availability of HAL release note

Posted on March 25, 2015 at 15:26Hello, I just came accros a new STM32 HAL version (driver dated 09 March 2015, version V1.3.0). Where can I find a description of changes compared to previous version(s)? Thanks.

stst9193 by Associate II
  • 2638 Views
  • 6 replies
  • 0 kudos

STM32CubeMX and LTDC configurator

Posted on March 27, 2015 at 09:16not working correctly setup window LTDC after opening already saved project(see. screenshot)after generating the project is not the correct parameters are passed to the C-project:(  

0690X00000603RxQAI.jpg

Can I use DSP lib with STM32L151?

Posted on March 30, 2015 at 08:08Can I use CMSIS-DSP  Verison 1.4.1 with STM32L151? I have it from the STM32F4 downloads and it is not available in the STM32L downloads, but it says it fits Cortex-M3. (library arm_cortexM3l_math.lib) #arm-cmsis-d...

igal by Associate II
  • 1690 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.