STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Pausing hardware OC

Posted on April 06, 2015 at 21:06I have a chain of 3 timers with TIMA -> TIMB -> TIMC.When TIMB is triggered it creates a pulse on an output pin via OPM. It then triggers TIMC to do an IC on its counter.What I want to do is to be able to programatic...

dibs by Associate II
  • 708 Views
  • 0 replies
  • 0 kudos

SD card CMD16 CRC fail

Posted on April 06, 2015 at 08:55Hello,I am trying to use Cube generated code to SD card interface (1 bit SDIO) initialization starts ok but I always get CRC error at CMD16 at this code://----------------------/* Set block size for card if it is not...

Johanan1 by Associate II
  • 1263 Views
  • 1 replies
  • 0 kudos

DCMI to SRAM via DMA does not work

Posted on October 23, 2014 at 11:23 Hello, i have project where i need to capture image from MT9M001 camera, store it inside SRAM (2MB) and do some complex calculation on image. In order to make it work, i cropped image from 1280x1024 to 102...

STM32F2 Erasing Flash kicks out my Debugger (Raisonance R-Link)

Posted on April 03, 2015 at 08:26Hi thereI have a slightly irritating issue where I am erasing a block of flash memory and while erasing it always kicks my debugger out.  I get a ''Debugger has lost communication message''I am using an STM32F207VCT6...

grant by Associate III
  • 1533 Views
  • 3 replies
  • 0 kudos

datasheet not user friendly

Posted on April 03, 2015 at 15:09hello, i was happy to know ST was offering very broad controller series line at very cost. i was very disappointed and felt the heat when i started using its datasheets. though it gives bulk of information it's certa...

kumaresh by Associate II
  • 2483 Views
  • 4 replies
  • 0 kudos

what is mean of Dhrystone ?

Posted on April 03, 2015 at 19:23hi everyone what is mean of 1.25 DMIPS(Dhrystone 2.1) is it DMIPS equal to Dhrystone milion instruction per secod? if yes please explain for me how execute 1.25DMIPS with arm core and pipeline i read a manual of ar...

os1361 by Associate II
  • 1775 Views
  • 3 replies
  • 0 kudos

Backup sram. Does the RTC have to also running

Posted on April 04, 2015 at 05:07Hi I want to save a Flag during a reboot on STM32F429IAt Main()I have  uint32_t bt; HAL_Init();  /* Configure the system clock to 180 Mhz */   SystemClock_Config();    __PWR_CLK_ENABLE();   HAL_PWR_EnableBkUpAccess...

brett23 by Associate II
  • 825 Views
  • 1 replies
  • 0 kudos

Trouble printing float number normally

Posted on April 03, 2015 at 21:15Attached is my modification of tiny_printf.c where I simply added float printing function (case 'f'). By default, the decimal points is 6. Below are floats I tried to print: Float                                    ...

chenping by Associate II
  • 2713 Views
  • 3 replies
  • 0 kudos

Trouble with UART Interrupt with IMU

Posted on April 02, 2015 at 19:59After extracting IMU from the demonstration project (merely leave out USB setting), now I face another issue is that whenever I tried to activate interrupt setting for UARTs, it hangs. (The circular LED_toggle indica...

chenping by Associate II
  • 2551 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.