STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32f407 TIM1 and TIM8 sync

Posted on March 14, 2015 at 15:18 Hello I'm trying to synchronize TIM1 and TIM8 (slaves) via TIM2 (master).. I checked the manual and says it can be done (p. 554/1710).. Although TIM2 works fine, TIM1 and TIM8 are off.. Please check my co...

zarkscon by Associate II
  • 7984 Views
  • 24 replies
  • 0 kudos

STM32F103 SmartCard Question

Posted on April 03, 2015 at 01:34I am trying to create a smartcard driver on the STM32F103.  I am using USART3, and the ST8024CTR interface chip.My problem is that I can read the cards (with a hack of a workaround), but cannot write to them.  What i...

jwormsley by Associate III
  • 1734 Views
  • 2 replies
  • 0 kudos

Scatter Brain

Posted on March 31, 2015 at 14:32I have a bootloader which needs to read an 8 byte char array from the application area to identify it's version information. So bootloader is located at 0x08000000Application firmware at :   0x08020000the char array ...

joe by Associate III
  • 2148 Views
  • 4 replies
  • 0 kudos

how to use ISER register in cortex-m4 core

Posted on April 03, 2015 at 10:48thanks to read this.i want to activate NVIC based on cortex-m4 core.but i am struggling to use Interrupt Set Enable register(ISER).pls anyone explain about NVIC in cortex M4 core and how i can use this.          than...

STM32F3 Discovery + LCD PCD8544 (Nokia 5110)

Posted on April 03, 2015 at 02:00Hey, I'm trying to get the PCD8544 working with my STM32F3 and I used this codehttp://stm32f4-discovery.com/?wpdmdl=1766that i found on this page http://stm32f4-discovery.com/pcd8544-nokia-33105110-lcd-stm32f429-disc...

mr by Associate
  • 1496 Views
  • 0 replies
  • 0 kudos

What's ETH_PPS_OUT in STM32F4x9 MAC.

Posted on September 12, 2013 at 21:48In ethernet MAC block, Port PB5 is assigned as ETH_PPS_OUT. I searched for a while and can find the usage of it. Is it MII_TX_ER?Sink.

tonyyu by Associate II
  • 1445 Views
  • 2 replies
  • 0 kudos

STM32L communication between 2 USART

Posted on March 25, 2015 at 17:39Hello all, I 'm novice and using STM32L152RE to do a communication between 2 USARTs I use USART2 for recieving GPS Data and I would like to echo all recievied data without parsing on PC Terminal by using USART3 bu...

kitjazax by Associate II
  • 5216 Views
  • 12 replies
  • 0 kudos

INTERFACE STM32 TO SRAM USING GPIO PINS

Posted on April 01, 2015 at 13:39Hi all,        We are trying to interface a 4M  SRAM (IS62WV25616ALL) to STM32F407IGT6 through GPIO Pins of the controller. We are able to write data sucessfully into the SRAM but we are facing difficulty in READING ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.