2015-04-14 12:55 AM
Hello
I have a nucleo STM32F103, I put a external clock of 25MHz.How can i read a analog signal conected in PB8?Someone can help me??Best regards #analog-input #nucleo-f103rb2015-04-14 5:21 AM
- set ADC configuration, enable adc channels, GPIO set as ''analog mode''
- set DMA channel configuration - transfer analog value to memory through DMA2015-04-14 6:20 AM
ADC analog channels have fixed pin assignments, unlike other peripherals which may have a choice of pins. PB8 is not an ADC channel.
Read the data sheet Section 3 Pin Assignments table and choose an appropriate pin e.g., PA1. Whichever peripheral library you are using will have ADC examples you can adapt for your project. Cheers, Hal2015-04-16 9:40 AM
2015-04-16 10:50 AM
Download the STM32F1 firmware library, there are ADC examples in that.
http://www.st.com/web/en/catalog/tools/PF257890
Ignore the Cube messaging, go to the red download button at the bottom.Not sure it's going to be useful for a 25 MHz signal, but that's either poorly expressed, or unrelated.You have an F103 or F105 part?2015-04-16 10:54 AM
The STM32028 examples should work on your nucleo with simple adaptation.
PB1 is ADC123 channel 9. None of the 7 examples in STM32028 use Channel 9. Which of the 7 examples are you using? Did you change the example channel to channel 9? Unless we see the code, we can only guess what is wrong. Regards, Hal2015-04-16 11:23 PM
Hello
All right Clive1: I have a Nucleo-F103RB but i changed the microcontroller and i put a STM32F I put a external clock at 25MHz. It is very similar to my final product Baird.hal.001: I am using the example with this path ''stsw-stm32028\STM32F10x_AN3116_FW_V1.0.0\Project\ADC Modes\SingleChannelContinuous'' I changed GPIO_ConfigurationGPIO_InitTypeDef GPIO_InitStructure;
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AIN;
GPIO_Init(GPIOB, &GPIO_InitStructure);
And now I chaged ADC_Channel_14 for ADC_Channel_9
Now all work.
I only have a final question.
can i use Port PB8 for analog adquisition???
Best regards
2015-04-17 3:33 AM
I only have a final question. Can i use Port PB8 for analog acquisition???
Thehttp://www.st.com/st-web-ui/static/active/en/resource/technical/document/datasheet/CD00220364.pdf
says it's not connected to an ADC, so no. Didn't Hal already mention that?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.