STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

help with timers

Posted on April 15, 2015 at 09:49I just created this simple project for an STM32F429 discovery board: 1) TIM1 is configured to produce a square waves on OC2 (PA9) 2) TIM2 is configured to use the ETR pin as clock source (PA5) 3) USB periodically sen...

infor by Associate III
  • 766 Views
  • 2 replies
  • 0 kudos

I2C Addr bit not set on 401 Discover Board

Posted on April 20, 2015 at 10:03Hi All,Please see below I2C protocal:I am using STM32F401 Discover Board, the slave is on board CS43L22, the address is 0x94.I try to send 0x01 to register 0x02: Single_WriteI2C(0x02,0x01), but only send out address,...

0690X000006059sQAA.png

Where do I begin?

Posted on April 18, 2015 at 03:00Hi all,I'm coming from the PICmicro world, and thought I'd get into ARM processors, so picked up an STM32L100C-DISCO.  I want to understand the basics -- for example, how to create a simple program to blink an LED.I ...

arm_dude by Associate II
  • 1791 Views
  • 6 replies
  • 0 kudos

Bitmap Converter, transparency and compression

Posted on April 21, 2015 at 00:30 Hi folks, I'm using Bitmap Converter (BmpCvtST.exe, v5.26, STemWin package) to convert images for display. Ordinarily when I save I select the ''High color [565] compressed'' output format and all is well. At...

hbarta2 by Associate III
  • 1104 Views
  • 0 replies
  • 0 kudos

STM32F103 EXTI not firing?

Posted on April 20, 2015 at 15:50Written this code many times. No clue why it is not working. See any obvious errors?//CODE FOR INIT. Note that APB2 clocks are initialized for ports  GPIO_InitTypeDef GPIO_EXTI0;   GPIO_EXTI0.GPIO_Pin = GPIO_Pin_7;  ...

STMCube IAR simple GPIO

Posted on April 20, 2015 at 19:36I'm migrating from PIC32s, so bear with me please.  I'm trying to get up to speed on the STM32 using the Cube examples in EWARM.  I'll try to keep this simple (I apologize, I don't know the syntax for code tags in th...

joe2399 by Associate II
  • 1502 Views
  • 3 replies
  • 0 kudos

Stuck in CAN TX Interrupt

Posted on April 20, 2015 at 20:36 I am currently have intermittent issue where I am getting stuck in ''void USB_HP_CAN_TX_IRQHandler(void)'', Everything works well from minutes to hours then I notice my CAN traffic stops, currently I TX one mess...

ebommer by Associate II
  • 1007 Views
  • 0 replies
  • 0 kudos

Capturing GPS Seconds Pulse STM32F1xx

Posted on April 20, 2015 at 10:33Hi, i have an external GPS signal that delivers seconds pulses (a short pulse every second). My goal is to count seconds in SW and trigger some actions every X seconds. Question a) I intend to use EXTI interrupt on e...

stm32cubef4 camera project for stm324xg_eval board

Posted on April 20, 2015 at 10:50HelloAccording to the page 18 of the ov2640 datasheet(version 1.6), device slave address is 0x60 for write and 0x61 for read, but in the camera_to_usbdisk project, only the write address is defined and used for both ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.