STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Timer interrupt Handler

Posted on April 17, 2015 at 17:51Hello.I have Using One of the example Program that port UCOS on STM32F4 Devices.I have One problem. When I activate Timer in one the tasks, The Timer is Working in a right way(example is on the blinking LED). but i w...

Counterfeit IC?

Posted on April 08, 2015 at 13:07Hi all,I�m designing a STM32F107VCT based embedded system. Unfortunately I�ve several problems with this part. For example the part wasn�t program correctly (Verification failed), and when I removed and soldered anot...

rezaxyz by Associate II
  • 1682 Views
  • 4 replies
  • 0 kudos

APB1/TIM2 clock

Posted on April 03, 2015 at 20:02How to find out APB1 clock frequency? I want to know TIM2 clock, which is connected to APB1. I use STM32F103 and standard peripheral library.Thank you.

hospodar by Associate III
  • 8937 Views
  • 12 replies
  • 1 kudos

DAC output range when buffer ON

Posted on April 18, 2015 at 06:47Hello,I have read the datasheet of stm32f407 about the DAC output range. When buffer on, the min DAC_OUT is 0.2V and max DAC_OUT is VDDA-0.2V.However, I get 0.069V at 0x000 and 3.272V at 0xfff rather than 0.2V and 3....

Independent Watchdog, Instruction before reset

Posted on April 18, 2015 at 10:08Hello,I'm running an Cube project with FreeRTOS, with iWDT enabled, on STM32L1 and debugging on IAR.iWDT is being cleared in its own thread, with the same priority as the other threads.No thread is a blocking thread....

George.P by Associate III
  • 2772 Views
  • 4 replies
  • 0 kudos

How to use STM32CubeF4 ?

Posted on April 14, 2015 at 11:46Hi Guys, Does anyone know how to use STM32CubeF4 with STM32F4 Discovery board ? Is it similar like using Keil ? Any clues please ? Thanks

STM32429I-EVAL camera not working

Posted on December 02, 2013 at 08:36I am trying to use the camera on STM32429I-EVAL, but cannot make it work. I took some code from Std-Periphs 1.3.0 which should demo the camera for 437, adapted it to start the camera on my board, but still cannot ...

HAL, cube MX, 411RE, SDIO microSD, FatFS Problem

Posted on April 19, 2015 at 23:36 I have a uSD card on a custom shield conected by SDIO (PC12, PC8, PD2 lines) I debug software and hardware (with my oscilloscope). I focus on this function static HAL_SD_ErrorTypedef SD_Initia...

SDIO CTIMEOUT: Command response timeout

Posted on April 20, 2015 at 01:44I'm using library only as a reference, so am writing simple test codes to understand guts of STM32F4xx. It is turn of SDIO.So far I'm able to read and write single block to SDHC card. My question to you is what shoul...

Changing DC on a PWM output with HAL

Posted on April 19, 2015 at 02:13Hello, I'm using a nucle 411 to test a RC servo driver. Si I configure 4 TIM3 channel to output PWM signal. Everithing is Ok, except that I can't finde a function to change PWM Duty Cycle. Is there any? BR!

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.