STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Is the MOSI pin in high impedance during a SPI read operation?

Posted on May 04, 2015 at 13:56Hello,My question is very simple. I'm wandering whether or not we can configure the MOSI/MISO pin as normal GPIO and set them in high impedance while a SPI communication is ongoing (just for clock generation for exampl...

darko by Associate
  • 1392 Views
  • 2 replies
  • 0 kudos

CubeMX, FreeRTOS and GPIO ??

Posted on April 27, 2015 at 07:42 Guys, I tried to test blinking LED using RTOS and cubemx, but can't make it until now ? what do I miss here ? Please have a look on the main.c .. Thanks for reading and giving a clues...

ADC channel reading

Posted on January 23, 2013 at 16:16Hi guys,I'm using two channels of ADC1 to convert two different inputs, i'm using the interrupt mode of End Of Conversion. I don't know how to get these values into two different variables.Please take a look at my ...

sherif by Associate II
  • 2803 Views
  • 6 replies
  • 0 kudos

High current consumption and MSI working in stop mode

Posted on November 07, 2012 at 17:33Hi, I'm working wih STM32L152 evaluation board, and i'm trying to make the MCU to enter stop mode. Though it seems like the MCU is stoping, I'm still woried about two things: 1. The MCU's current consumption is ab...

amirf by Associate
  • 2052 Views
  • 4 replies
  • 0 kudos

STM32F429 - Discovery - STMemWIN example

Posted on May 04, 2015 at 08:57Hi all,I try to understand the STMemWin example from the KEIL Library for the STM32F429 - Discovery Board and to make a own one step by step, now the point apears where i get suck with a problem. The Display is only Wh...

Need help with TIM15 of Stm32F051 and HAL

Posted on April 30, 2015 at 03:33Hi all,I want to measure a ~5ms signal at TIM15 Channel 1.Our examples and information I have dont work.Can somebody help me with sample HAL code? Thanks,Osto

Osto by Senior
  • 845 Views
  • 3 replies
  • 0 kudos

ADC artifacts in conti-mode STM32L100RC

Posted on April 29, 2015 at 23:18 Dear Community, I’ve investigated the ADC of the STM32L100RC (DISCO-Board) in continuous and in the triggered mode.In continuous mode I was able to reach a sample frequency of ~300 kHz which I investigated exp...

jogerh by Associate II
  • 1442 Views
  • 3 replies
  • 0 kudos

STM32F411 SPI2 - MPU6000 - Tx and Rx with DMA

Posted on May 04, 2015 at 01:37 I'm comunicating a nucleo board with a mpu6000 mems sensor, using CubeMX to make initialization code. It is working ok, but with just one issue. I have to write 0x3B|0x80 and a 16 0x00 (dummy bytes) and read b...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.