2015-05-03 4:37 PM
I'm comunicating a nucleo board with a mpu6000 mems sensor, using CubeMX to make initialization code.
It is working ok, but with just one issue. I have to write 0x3B|0x80 and a 16 0x00 (dummy bytes) and read back 16 bytes from sensor. I have a uint8_t dataOut[16] = {0x3B|0x80, 0,0,0,0....,0} The thing is that HAL_SPI_TransmitReceive_DMA send 3 times 0x3B|0x80 and so the data I've read is wrong. I solve this issue first sending HAL_SPI_Transmit 0x3B|0x80 and then calling to HAL_SPI_TransmitReceive_DMA. But I'm really would like erase SPI_Transmit. Does anybody know somthing about it?/* Peripheral DMA init*/
hdma_spi2_tx.Instance = DMA1_Stream4;
hdma_spi2_tx.Init.Channel = DMA_CHANNEL_0;
hdma_spi2_tx.Init.Direction = DMA_MEMORY_TO_PERIPH;
hdma_spi2_tx.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_spi2_tx.Init.MemInc = DMA_MINC_DISABLE;
hdma_spi2_tx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdma_spi2_tx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdma_spi2_tx.Init.Mode = DMA_NORMAL;
hdma_spi2_tx.Init.Priority = DMA_PRIORITY_LOW;
hdma_spi2_tx.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
HAL_DMA_Init(&hdma_spi2_tx);
__HAL_LINKDMA(hspi,hdmatx,hdma_spi2_tx);
hdma_spi2_rx.Instance = DMA1_Stream3;
hdma_spi2_rx.Init.Channel = DMA_CHANNEL_0;
hdma_spi2_rx.Init.Direction = DMA_PERIPH_TO_MEMORY;
hdma_spi2_rx.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_spi2_rx.Init.MemInc = DMA_MINC_ENABLE;
hdma_spi2_rx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdma_spi2_rx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdma_spi2_rx.Init.Mode = DMA_NORMAL;
hdma_spi2_rx.Init.Priority = DMA_PRIORITY_LOW;
hdma_spi2_rx.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
HAL_DMA_Init(&hdma_spi2_rx);
__HAL_LINKDMA(hspi,hdmarx,hdma_spi2_rx);
sensor continously make an interrupt at sample rate (200Hz) and on ISR:
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
uint8_t addr;
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_12, GPIO_PIN_RESET);
addr=0x3B|0x80;
// data[0]=0x3B|0x80;
HAL_SPI_Transmit(&hspi2, &addr, 1, 10);
HAL_SPI_Receive_DMA(&hspi2, data, 16);
// HAL_SPI_TransmitReceive_DMA(&hspi2, &addr, data, 17);
}
HAL_SPI_Receive_DMA calls to
HAL_SPI_TransmitReceive_DMA inside their code.
on SPI_DMA Tx complete I do:
void HAL_SPI_RxCpltCallback(SPI_HandleTypeDef *hspi)
{
int16_t tmp=0;
tmp=(data[6]<<8) | data[7];
tempC = (double)(tmp)/0 + 53;
X_accel = (int16_t)((data[0]<<8) | data[1])/160;
Y_accel = (int16_t)((data[2]<<8) | data[3])/160;
Z_accel = (int16_t)((data[4]<<8) | data[5])/160;
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_12, GPIO_PIN_SET);
}
BR!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.