2015-04-20 5:21 PM
Hi,
I connected only one qspi flash to the BK2_IOx pins of the STM32F446. Is it possible to use this flash as single-flash mode? Based on the STM32F446 datasheet, there's no QUADSPI_BK1_IO2 for 64 pins package, is it correct? Ari.2015-05-04 6:49 AM
Hi Ari,
1- To use one flash as single-flash mode, you can connect flash memory to BK1_IOx or BK2_IOx pins and select the FLASH memory to be addressed in single flash mode in the FSEL bit in QUADSPI control register (QUADSPI_CR).2- For the LQFP64 package, the Quad SPI is available with limited features, so it is correct: there is no QUADSPI_BK1_IO2.Sorry for answer delay ;)-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.