STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to use HAL_USART_Transmit ?

Posted on May 07, 2015 at 02:06 Hi Guys, How can I use HAL_USART_Transmit ? I've initialized USART1... And I want to transmit a test message on the task : void StartTask02(void const * argument) { /* USER CODE BEGIN St...

Overview of the STM32 IO ports? PWM?

Posted on May 06, 2015 at 18:55Currently in the investigative process of migrating PIC to STM32 I'm pretty early in on the process so go easy on me. My work is mostly CAN but also USB, some switches and LED work. PWM questions: 1. I see the STM32F1...

este00 by Associate II
  • 2233 Views
  • 2 replies
  • 0 kudos

USART application DELAY error on STM32F4

Posted on May 06, 2015 at 21:33I have develop an app and one button is sending the string A. However when i connect the STM32F407 and run the program it only can execute one command line instead of all command under the char A. Is there anyway to ta...

stm32f4 and vcp [com port doesn't show up correctly]

Posted on May 06, 2015 at 19:24Hi, I am trying to use stm32 USB by using the virtual port com.I installed the vcp's driver then downloaded the standard vcp example for stm32f4xx series from st. I opened then the device manager to check for the com p...

d4ng3r09 by Associate II
  • 1233 Views
  • 2 replies
  • 0 kudos

STM32F4Discovery Demo quit working

Posted on August 09, 2014 at 23:18The demo program no longer works on my board. I flashed the audio demo from the STM32F4DISCOVERY board firmware package. After playing with it for a while, I flashed the board with the Demonstration hex file from th...

sfugarino by Associate II
  • 3016 Views
  • 8 replies
  • 0 kudos

STM32 SPI problem

Posted on May 03, 2013 at 09:02I want to interface winbond W25Q64BV SPI flash with STM32F103VE running at 24MHz. I was able to perfectly read the status registers and ID's of flash using commands 0x05,0x35,0x9F,0x4B,0x90,0xAB. But I am not able to e...

CubeMX 4.7.1 not using STM32L1 1.2.0

Posted on May 06, 2015 at 00:27I updated CubeMX and installed the new 1.2.0 firmware for the STM32L1 family earlier today.  However, CubeMX won't migrate existing projects or create new projects using the new firmware package.  Even after deleting 1...

seth by Associate II
  • 1356 Views
  • 2 replies
  • 0 kudos

Confusion on STM32F407 DMA FIFO mode, Please help

Posted on May 04, 2015 at 06:42Hello everyone,Nowadays, I'm trying to figure out how the FIFO of DMA works. But get stumbled with the DMA memory to peripheral mode with FIFO enabled.Firstly, the STM32F4 ''RM0090 Reference manual'' P.219 ''Memory-to-...

sunnyqd by Associate II
  • 5729 Views
  • 10 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.