2015-05-06 12:33 PM
I have develop an app and one button is sending the string A. However when i connect the STM32F407 and run the program it only can execute one command line instead of all command under the char A. Is there anyway to tackle this problem? I KNOW IT IS RELATED TO DELAY PROBLEM. BUT HOW CAN I SOLVE IT BY PROGRAMMING? THANKS!!!
&sharpinclude ''stm32f4xx.h''&sharpinclude ''usart_config.h''&sharpinclude ''String.h''&sharpinclude ''config.h''&sharpinclude ''delay.h''void usart_lowLevelInit(){ GPIO_InitTypeDef GPIO_InitStructure; /**************************GPIO Configuration*****************************/ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE); RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART3, ENABLE); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10 | GPIO_Pin_11; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOC, &GPIO_InitStructure); /* Connect USART pins to AF */ GPIO_PinAFConfig(GPIOC, GPIO_PinSource10, GPIO_AF_USART3); GPIO_PinAFConfig(GPIOC, GPIO_PinSource11, GPIO_AF_USART3); //*************************USARTx configuration ***************************** USART_InitTypeDef USART_InitStructure; /* USARTx configuration -------------------------------/ / * USARTx configured as follow: - BaudRate = 9600 baud - Word Length = 8 Bits - Two Stop Bit - Odd parity - Hardware flow control disabled (RTS and CTS signals) - Receive and transmit enabled */ USART_InitStructure.USART_BaudRate = 9600; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; USART_Init(USART3, &USART_InitStructure); USART_Cmd(USART3, ENABLE); /*USART_ITConfig(USART3, USART_IT_TC, ENABLE);*/ USART_ITConfig(USART3, USART_IT_RXNE, ENABLE); //***************************Interruption Config*********************************** NVIC_InitTypeDef NVIC_InitStructure; /* Configure the NVIC Preemption Priority Bits */ //NVIC_PriorityGroupConfig(NVIC_PriorityGroup_0); /* Enable the USART3 Interrupt */ NVIC_InitStructure.NVIC_IRQChannel = USART3_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); }//------------------Fonction de Reception ---------------------------------extern __IO uint8_t cursor,flag;extern __IO char buffer[20],result[20];extern __IO char c;void usart_receive(char c){ if (c=='A') { moteur2(1550); delay_nms(100); moteur17(1500); delay_nms(100) ; moteur3(2150); delay_nms(100) ; moteur18(1300); delay_nms(100) ; moteur2(1750); delay_nms(100); moteur17(1200); delay_nms(100) ; moteur8(1200); delay_nms(100); moteur11(1600); delay_nms(100) ; moteur12(500); delay_nms(100) ; moteur9(1400); delay_nms(100); moteur8(1500); delay_nms(100); moteur11(1300); delay_nms(100) ; moteur5(1500);delay_nms(100); moteur14(2100); delay_nms(100); moteur15(1000); delay_nms(100) ; moteur6(1100); delay_nms(100) ; moteur5(1800); delay_nms(100); moteur14(1800); delay_nms(100); moteur3(1850); moteur18(1600); moteur12(900); moteur9(1000); moteur15(1400); moteur6(700); } else if (c=='B') { moteur2(1550); delay_nms(100); moteur17(1500); delay_nms(100) ; moteur3(1650); delay_nms(100) ; moteur18(1700); delay_nms(100) ; moteur2(1750);delay_nms(100); moteur17(1200); delay_nms(100) ; moteur8(1200); delay_nms(100); moteur11(1600); delay_nms(100) ; moteur12(1200); delay_nms(100); moteur9(700); delay_nms(100); moteur8(1500); delay_nms(100); moteur11(1300); delay_nms(100) ; moteur5(1500);delay_nms(100); moteur14(2100); delay_nms(100); moteur15(1800); delay_nms(100) ; moteur6(300); delay_nms(100) ; moteur5(1800); delay_nms(100); moteur14(1800); delay_nms(100); moteur3(1850); moteur18(1600); moteur12(900); moteur9(1000); moteur15(1400); moteur6(700);} } /*----------Dans Le Fichier stm32f4xx_it on ajoute----------------extern char c;extern __IO uint8_t cursor;extern __IO char buffer[64],result[64];void USART3_IRQHandler(void){ c= (char)USART_ReceiveData( USART3);usart_receive(c);} *///------------------Dans Le fichier Main---------------------------- //usart_lowLevelInit()//if (flag==0) flag=1;//&sharpinclude ''usart_config.h'' #stm32 #stm32f4 #usart2015-05-06 12:51 PM
Is there anyway to tackle this problem?
I guess there's static analysis and dynamic analysis, for the latter you could use a debugger and understand what's going on.From a static perspective you've got a LOT going on during the IRQ, it really should do it's work quickly and leave. You have a lot of delays, possibly dependent on other interrupts, which are unable to execute because you don't leave yours.2015-05-06 2:09 PM
thanks!!! but is there anyway that i can change from the configuration as t solve this problem? thanks!
2015-05-06 5:45 PM
You could stop using an IRQ based counter for delays, and use a hardware timer/counter instead. Waiting for it to transition through whatever milliseconds, or microseconds constitute the delay.
You could stop running code under interrupt, and instead run it in a different task, or in a foreground loop, or as a state machine, after you recognize you've received the command character. A state machine might be useful if you can step through the sequence every millisecond. Also, I'd prefer you didn't edit questions after they have received an answer, it damages the integrity of the thread.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.