STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Write ISR in uCOSII

Posted on May 07, 2015 at 22:01HII am Using stm32f40x and one of the UcosII from Micrium site.I have a problem to enable interrupts in uCOS. I use the BSPxx Functions to set vector and enable interrupts but it did not worked well.I would be very tha...

SDIO + DMA on stm32f103

Posted on May 07, 2015 at 15:56Hi everyone,I am using SDIO interface to write to SD card without using DMA. I am writing about 300 bytes of data at 50Hz. The problem is that with current implementation it slows down the code.Thats why I am thinking ...

STM32F103 TIM2 configuration

Posted on May 06, 2015 at 19:21 Hi there..! sorry if my question seems duplicate but I dont know what's wrong, I want to set TIM2 interrupt to 1 ms without success. this is my clock configuration #define __RCC_CR_VAL 0x010...

STM32F411 Virtual Com Error (Code 10)

Posted on May 06, 2015 at 15:05Hello,I am using the Cube to configure the micro's USB OTG as a virtual com device.  However, when I plug this USB into my Windows 7 PC, the driver on the PC reports that the device cannot be started (code 10).  I have...

nmadinger by Associate II
  • 3350 Views
  • 7 replies
  • 0 kudos

F103: ADC injected scan mode question

Posted on September 24, 2014 at 02:19Hello,I'm implementing a high power buck converter using STM32F103C8. I need to measure voltage on 4 channels during each PWM period. I figured, that i will use ADC injected mode for this. Since PWM is being gene...

Problems using DMA on DAC channel 2

Posted on May 07, 2015 at 11:17I am experimenting STM32F429 on a discovery board. After creating set board settings with STM32CubeMX, I created a few lines to generate a wave on DAC channel 2 using DMA. Everything seems correct in the registers, but...

infor by Associate III
  • 1109 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.