STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 Interrupt priorities and preemption

Posted on July 18, 2013 at 15:47 Hi, I have a problem where I cannot get a higher priority interrupt to interrupt a lower priority one. My understanding is that this should 'just work' so I'd really appreciate your input on this... I've creat...

gw by Associate II
  • 11480 Views
  • 6 replies
  • 0 kudos

stm32f4 read data from pc's com port

Posted on May 10, 2015 at 15:40 I managed to send via stm32f4 data using usb and vcp.What i am trying to do now is to read data from pc .In order to check what is read through usb i send it again to the pc. My problem is that the board seems ...

d4ng3r09 by Associate II
  • 1976 Views
  • 3 replies
  • 0 kudos

why is the following SPI implementation not working?

Posted on May 08, 2015 at 22:03Hello,I have trouble to communicate with a BlueNRG device. I�ve tracked it down to my SPI implementation. Assumed I want to have a �usual�, full duplex SPI master interface on a STM32L152, using CMSIS I initialize the ...

torsten2 by Associate II
  • 1525 Views
  • 3 replies
  • 0 kudos

STM32F10x standard peripheral library v3.6.1

Posted on January 29, 2015 at 13:22Here is the official place to download the latest version of SPL for STM32F10x: http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1743/PF257890SPL version is 3.5.0 from 2011 and the CMSIS version included in...

DAC Signals Generation

Posted on April 27, 2015 at 19:44The original post was too long to process during our migration. Please click on the attachment to read the original post.

mka500 by Associate
  • 1664 Views
  • 3 replies
  • 0 kudos

Stm32F429I-Discovery Board stm32cubef4\STM32Cube_FW_F4_V1.5.0\Projects\STM32F429I-Discovery\Demonstrations_ Example

Posted on May 09, 2015 at 14:25i am using this example  stm32cubef4\STM32Cube_FW_F4_V1.5.0\Projects\STM32F429I-Discovery\Demonstrationsi want to change the Icons in the Demo Applicationwhat type of Tool am i required to convert bmp to c fileHere the...

senthil by Associate II
  • 942 Views
  • 2 replies
  • 0 kudos

DMA connections in stm32f103c8

Posted on May 10, 2015 at 07:31Helloaccording to it's datasheet and reference manual, only DMA1 controller is active in this device.Is GPIO peripheral connected to DMA streams in this device so that GPIO to memory transfers can be implemented?Thanks...

Startup Files with different chipsets

Posted on April 20, 2015 at 23:28Hi all,I have a legacy boot loader that was run on an STM32F407.  It was located at 0x08000000 and my main application is located at 0x08020000.  I have seen a strange behaviour when I compile my main application cod...

FSMC do not work

Posted on May 10, 2015 at 07:08I crate a project with stm32cube my chip is stm32f103zc i enable fsmc for lcd interface and 16 bit data address and A0 for register select . this function HAL_SRAM_Read_16b(&hsram1,&send_address,send_buffer,10); do no...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.