STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

To get data from Invensense MPU9250 with I2C

Posted on May 26, 2015 at 13:25I'm trying to get data from Invensense MPU9250 with I2C on SC1 of stm32w108.These are connected each other with 10k ohm register.But it doesn't get data.I coded as below.Please tell me how to fix.void SCinit(){        ...

kano by Associate
  • 818 Views
  • 0 replies
  • 0 kudos

What is the maximum frequency of STM32F4's PWM?

Posted on May 26, 2015 at 07:11I would like to use the PWM as clock source for other device. so I want to know the maximum frequency of PWM. As faster the frequency of PWM signal increase, the more the shape of PWM signal become to triangle signal. ...

0690X00000605HGQAY.png 0690X00000605HLQAY.png 0690X00000605HMQAY.png 0690X00000605B9QAI.png
just4u78 by Associate II
  • 1888 Views
  • 1 replies
  • 0 kudos

Debug step-by-step with Watchdog enable !

Posted on May 26, 2015 at 09:49Hello,I am debugging step-by-step my project on stm32f103vd, using CooCox CoIDE, and ST-LinkV2.when I enable whatchdog, the system go then to Reset_DefaultHandler(). I think that's normal no ?and how I can debug step-b...

Where is UM1525 gone ?

Posted on April 27, 2015 at 14:42The user manual for the STM32F051 discovery (named UM1525) seems to be gone from the respective http://www.st.com/web/catalog/tools/FM116/SC959/SS1532/LN1848/PF253215. Some kind of meltdown ? #um1525

AvaTar by Lead
  • 1617 Views
  • 3 replies
  • 0 kudos

SPI problem reading ADC

Posted on May 18, 2015 at 10:19 I'am using three MAX11210 with a STM32L151VDT6 controller via SPI. I only want to read out the CTRL3 register which is by default 0x1E. If i read out the ADCs behind one another i read 0x1E, 0x1E and 0x1F... but n...

juergen23 by Associate II
  • 2057 Views
  • 3 replies
  • 0 kudos

STM32F103 Usart receive strange problem

Posted on May 25, 2015 at 16:45 Hi there, I try to send data from PC to my stm32 board using RS232 but each time I send data to stm I get exactly same strange other data for sample: if i send 0x12 i receive 0xc4 always and if i s...

Question about memory mapping stm32F407VE

Posted on May 24, 2015 at 16:52Hello, i have a question, since i dont have much experience working with flash... The 32F407VE is 512kbytes flash size,   but when trying to read the content of the flash with ST LINK application, the flash range is on...

Bogdan by Senior
  • 2528 Views
  • 6 replies
  • 0 kudos

RTC-STM32F0 wakeup timer with LSE

Posted on May 24, 2015 at 20:48I've startup a board using STM32F072 ( new with ST :) ) ,but cannot get the RTC wake up timer to work, i can see the RTC  Registers are moving using LSE 32K crystal in debug mode, thus RTC->DR increase every second.i w...

Failing to set up USART DMA TX

Posted on May 22, 2015 at 15:33 Hello, Can anyone help in pinpointing where and what I'm doing wrong when seting up USART DMA TX transmission. Working with STM32L152RB (STM32L discovery) and trying to setup USART1_TX overDMA1_Channel4,USA...

lauris by Associate III
  • 1505 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.