2015-05-24 11:48 AM
I've startup a board using STM32F072 ( new with ST :) ) ,but cannot get the RTC wake up timer to work, i can see the RTC Registers are moving using LSE 32K crystal in debug mode, thus RTC->DR increase every second.
i want:to use the 1 second interrupt to activate some flags and to awake from STOP modethis is the startup code generated with Cube. RTC_TimeTypeDef sTime; RTC_DateTypeDef sDate; /**Initialize RTC and set the Time and Date */ hrtc.Instance = RTC; hrtc.Init.HourFormat = RTC_HOURFORMAT_24; hrtc.Init.AsynchPrediv = 127; hrtc.Init.SynchPrediv = 255; hrtc.Init.OutPut = RTC_OUTPUT_DISABLE; hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH; hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN; HAL_RTC_Init(&hrtc); sTime.Hours = 0; sTime.Minutes = 0; sTime.Seconds = 0; sTime.SubSeconds = 0; sTime.TimeFormat = RTC_HOURFORMAT12_AM; sTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE; sTime.StoreOperation = RTC_STOREOPERATION_RESET; HAL_RTC_SetTime(&hrtc, &sTime, FORMAT_BIN); sDate.WeekDay = RTC_WEEKDAY_MONDAY; sDate.Month = RTC_MONTH_JANUARY; sDate.Date = 1; sDate.Year = 0; HAL_RTC_SetDate(&hrtc, &sDate, FORMAT_BIN); /**Enable the WakeUp */ HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, 16, RTC_WAKEUPCLOCK_RTCCLK_DIV16);// NVIC_SetPriority(RTC_IRQn, 0); // NVIC_EnableIRQ(RTC_IRQn); // - with or without this the result is the same the interrupt never enters.// -------------------------- this is the interrupt, that never enters ----------------------void RTC_IRQHandler(void){ RTC->ISR &=~ RTC_ISR_WUTF; TFlags1S.Val=0xFFFF;}2015-05-25 6:23 PM
Hi, I don't use Cube/HAL but it sounds like you may be missing an ''enable wakeup int'' somewhere in your initialization. Have you checked the actual contents of the RTC_CR and RTC_ISR registers while your code is running ? I'd check the WUTIE, and maybe WUTE and WUTF bits.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.