2015-06-05 2:29 AM
hej,
i am getting a wrong values when i measuring the signal in input capture mode.can anyone help me what i am doing wrong and also i am new to this .i am using stm32f407vg the below oen is intialization. /new one TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; TIM_TimeBaseStructure.TIM_Prescaler =168 - 1; TIM_TimeBaseStructure.TIM_Period = 65535; TIM_TimeBaseStructure.TIM_ClockDivision = 0x0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM1, &TIM_TimeBaseStructure); GPIO_InitTypeDef GPIO_IniStructure; NVIC_InitTypeDef NVIC_IniStructure; RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM1, ENABLE); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOE, ENABLE); GPIO_IniStructure.GPIO_Pin = GPIO_Pin_11; GPIO_IniStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_IniStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_IniStructure.GPIO_OType = GPIO_OType_PP; GPIO_IniStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOE, &GPIO_IniStructure); GPIO_PinAFConfig(GPIOE, GPIO_PinSource11, GPIO_AF_TIM1); //timer alternative function mapping NVIC_IniStructure.NVIC_IRQChannel = TIM1_CC_IRQn; //TIM1 Capture Compare Interrupt NVIC_IniStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_IniStructure.NVIC_IRQChannelSubPriority = 1; NVIC_IniStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_IniStructure); TIM_ICInitTypeDef TIM_ICInitStructure; TIM_ICInitStructure.TIM_Channel = TIM_Channel_2; TIM_ICInitStructure.TIM_ICPolarity = TIM_ICPolarity_Rising; TIM_ICInitStructure.TIM_ICSelection = TIM_ICSelection_DirectTI; TIM_ICInitStructure.TIM_ICPrescaler = TIM_ICPSC_DIV1; TIM_ICInitStructure.TIM_ICFilter = 0x0; TIM_ICInit(TIM1, &TIM_ICInitStructure); TIM_Cmd(TIM1, ENABLE); TIM_ITConfig(TIM1, TIM_IT_CC2, ENABLE); the below one has to give me proper value but i am not measuring the proper signal . void TIM1_CC_IRQHandler(void) { if(TIM_GetITStatus(TIM1, TIM_IT_CC2) == SET) { TIM_ClearITPendingBit(TIM1, TIM_IT_CC2); if(CaptureNumber == 0) { //sprintf(processcommand, ''%d'', IC3ReadValue2); //printf( ''IC3ReadValue2 %d \n'', IC3ReadValue1 ); //usart_SEND (USART6,processcommand); IC3ReadValue1 = TIM_GetCapture2(TIM2); CaptureNumber = 1; } else if(CaptureNumber == 1) { IC3ReadValue2 = TIM_GetCapture2(TIM1); //printf( ''IC3ReadValue2 %d \n'', IC3ReadValue2 ); if (IC3ReadValue2 > IC3ReadValue1) { Capture = 0; Capture = (IC3ReadValue2 - IC3ReadValue1); } else if (IC3ReadValue2 < IC3ReadValue1) { Capture = 0; Capture = ((0xFFFF - IC3ReadValue1) + IC3ReadValue2); } else { Capture = 0; } TIM1Freq = (uint32_t) SystemCoreClock / Capture; sprintf(processcommand, ''%d'', TIM1Freq); usart_SEND (USART6,processcommand); usart_SEND (USART6,''\n\r''); //TIM1Freq = (uint32_t) SystemCoreClock / Capture1; CaptureNumber = 0; } } } i am using timer 1 and the clock frequency of that is 168MHZ. thank you ..2015-06-05 6:12 AM
What is the nature of the signal you're trying to measure? Frequency, etc
What are the wrong/incorrect value you are getting vs expected? The 16-bit math in your routine is broken.2015-06-05 8:09 AM
I've got it working on 429 disco with both SPL and HAL libraries.
Measured pulse length with 6.24nS step up to 14 sec. PS frequency is 168MHz I can post you codes (later today)2015-06-05 8:19 AM
Probably not with 16-bit measurement/numbers.
2015-06-05 1:02 PM
#include ''stm32f4xx_hal.h''
#include ''usb_device.h'' #include ''usbd_cdc_if.h'' TIM_HandleTypeDef timM; TIM_HandleTypeDef timS; TIM_MasterConfigTypeDef m; TIM_SlaveConfigTypeDef s; TIM_IC_InitTypeDef ic; void Error_Handler(void) {HAL_GPIO_WritePin(GPIOG,GPIO_PIN_14,GPIO_PIN_SET); while(1){}} void EXTI0_IRQHandler(void) {if(HAL_GPIO_ReadPin(GPIOG,GPIO_PIN_14)==GPIO_PIN_RESET) {if(HAL_TIM_IC_Stop_IT(&timM,TIM_CHANNEL_1)!=HAL_OK)Error_Handler(); if(HAL_TIM_IC_Start_IT(&timM,TIM_CHANNEL_2)!=HAL_OK)Error_Handler();} else {if(HAL_TIM_IC_Stop_IT(&timM,TIM_CHANNEL_2)!=HAL_OK)Error_Handler(); if(HAL_TIM_IC_Start_IT(&timM,TIM_CHANNEL_1)!=HAL_OK)Error_Handler();} HAL_GPIO_TogglePin(GPIOG,GPIO_PIN_14); HAL_NVIC_ClearPendingIRQ(EXTI0_IRQn); HAL_GPIO_EXTI_IRQHandler(GPIO_PIN_0);} void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef *htim) {extern USBD_HandleTypeDef hUsbDeviceHS; extern TIM_HandleTypeDef timS; uint8_t buff_TX[128]; buff_TX[0]='0'; if(htim->Channel==HAL_TIM_ACTIVE_CHANNEL_1) {buff_TX[1]=1; buff_TX[2]=HAL_TIM_ReadCapturedValue(htim,TIM_CHANNEL_1)>>8; buff_TX[3]=HAL_TIM_ReadCapturedValue(htim,TIM_CHANNEL_1);} else {buff_TX[1]=2; buff_TX[2]=HAL_TIM_ReadCapturedValue(htim,TIM_CHANNEL_2)>>8; buff_TX[3]=HAL_TIM_ReadCapturedValue(htim,TIM_CHANNEL_2);} buff_TX[4]=TIM3->CNT>>8; buff_TX[5]=TIM3->CNT; buff_TX[6]=TIM9->CNT>>8; buff_TX[7]=TIM9->CNT; USBD_CDC_SetTxBuffer(&hUsbDeviceHS,&buff_TX[0],8); USBD_CDC_TransmitPacket(&hUsbDeviceHS); HAL_GPIO_TogglePin(GPIOG,GPIO_PIN_13);} int main(void) {HAL_Init(); RCC_OscInitTypeDef RCC_OscInitStruct; RCC_ClkInitTypeDef RCC_ClkInitStruct; __PWR_CLK_ENABLE(); __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1); RCC_OscInitStruct.OscillatorType=RCC_OSCILLATORTYPE_HSE; RCC_OscInitStruct.HSEState=RCC_HSE_ON; RCC_OscInitStruct.PLL.PLLState=RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource=RCC_PLLSOURCE_HSE; RCC_OscInitStruct.PLL.PLLM=8; RCC_OscInitStruct.PLL.PLLN=336; RCC_OscInitStruct.PLL.PLLP=RCC_PLLP_DIV2; RCC_OscInitStruct.PLL.PLLQ=7; HAL_RCC_OscConfig(&RCC_OscInitStruct); RCC_ClkInitStruct.ClockType=RCC_CLOCKTYPE_SYSCLK|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2; RCC_ClkInitStruct.SYSCLKSource=RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.AHBCLKDivider=RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider=RCC_HCLK_DIV4; RCC_ClkInitStruct.APB2CLKDivider=RCC_HCLK_DIV2; HAL_RCC_ClockConfig(&RCC_ClkInitStruct,FLASH_LATENCY_5); __GPIOH_CLK_ENABLE(); __GPIOG_CLK_ENABLE(); GPIO_InitTypeDef initGPIO; initGPIO.Pin=GPIO_PIN_13|GPIO_PIN_14; initGPIO.Mode=GPIO_MODE_OUTPUT_PP; initGPIO.Pull=GPIO_PULLDOWN; initGPIO.Speed=GPIO_SPEED_LOW; HAL_GPIO_Init(GPIOG,&initGPIO); HAL_GPIO_WritePin(GPIOG,GPIO_PIN_13|GPIO_PIN_14,GPIO_PIN_SET); __GPIOA_CLK_ENABLE(); initGPIO.Pin=GPIO_PIN_0; initGPIO.Mode=GPIO_MODE_IT_FALLING; initGPIO.Pull=GPIO_NOPULL; HAL_GPIO_Init(GPIOA,&initGPIO); HAL_NVIC_SetPriorityGrouping(NVIC_PRIORITYGROUP_0); HAL_NVIC_SetPriority(EXTI0_IRQn,4,1); HAL_NVIC_EnableIRQ(EXTI0_IRQn); __GPIOB_CLK_ENABLE(); MX_USB_DEVICE_Init(); HAL_GPIO_WritePin(GPIOG,GPIO_PIN_13|GPIO_PIN_14,GPIO_PIN_RESET); __GPIOE_CLK_ENABLE(); GPIO_InitTypeDef GPIO_InitStruct; GPIO_InitStruct.Pin=GPIO_PIN_5|GPIO_PIN_6; GPIO_InitStruct.Mode=GPIO_MODE_AF_PP; GPIO_InitStruct.Pull=GPIO_PULLUP; GPIO_InitStruct.Speed=GPIO_SPEED_HIGH; GPIO_InitStruct.Alternate=GPIO_AF3_TIM9; HAL_GPIO_Init(GPIOE,&GPIO_InitStruct); HAL_NVIC_SetPriority(TIM1_BRK_TIM9_IRQn,5,5); HAL_NVIC_EnableIRQ(TIM1_BRK_TIM9_IRQn); __TIM9_CLK_ENABLE(); timM.Instance=TIM9; timM.Init.Period=0xffff; timM.Init.Prescaler=0; timM.Init.ClockDivision=TIM_CLOCKDIVISION_DIV1; timM.Init.CounterMode=TIM_COUNTERMODE_UP; if(HAL_TIM_IC_Init(&timM)!=HAL_OK)Error_Handler(); __TIM3_CLK_ENABLE(); timS.Instance=TIM3; timS.Init.Period=0xffff; timS.Init.Prescaler=0; timS.Init.ClockDivision=TIM_CLOCKDIVISION_DIV1; timS.Init.CounterMode=TIM_COUNTERMODE_UP; if(HAL_TIM_IC_Init(&timS)!=HAL_OK)Error_Handler(); ic.ICPrescaler=TIM_ICPSC_DIV1; ic.ICFilter=0; ic.ICPolarity=TIM_ICPOLARITY_FALLING; ic.ICSelection=TIM_ICSELECTION_INDIRECTTI; if(HAL_TIM_IC_ConfigChannel(&timM,&ic,TIM_CHANNEL_1)!=HAL_OK)Error_Handler(); ic.ICPolarity=TIM_ICPOLARITY_RISING; ic.ICSelection=TIM_ICSELECTION_DIRECTTI; if(HAL_TIM_IC_ConfigChannel(&timM,&ic,TIM_CHANNEL_2)!=HAL_OK)Error_Handler(); s.InputTrigger=TIM_TS_TI2FP2; s.SlaveMode=TIM_SLAVEMODE_RESET; if(HAL_TIM_SlaveConfigSynchronization(&timM,&s)!=HAL_OK)Error_Handler(); if(HAL_TIM_IC_Start_IT(&timM,TIM_CHANNEL_1)!=HAL_OK)Error_Handler(); if(HAL_TIM_IC_Start_IT(&timM,TIM_CHANNEL_2)!=HAL_OK)Error_Handler(); while(1){}} #ifdef USE_FULL_ASSERT void assert_failed(uint8_t* file,uint32_t line){} #endif2015-06-07 2:07 AM
clive, i am measuring 2khz sqaure wave signal...
i am getting random values ..whats meantby ''The 16-bit math in your routine is broken''....if possible can you post a sample programme ....thank you in advanceWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.