STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

[solved] STM32L151UC: SPI3 problem - no activity on pins

Posted on June 15, 2015 at 14:20Hello, I am trying to configure the SPI3 port of an STM32L151UC micro controller. I have tried several things but I see no output on the related pins. When using gpios instead of the AF of the SPI peripheral, I can ...

bxCAN Master vs Slave

Posted on June 12, 2015 at 14:20I would like to connect to my car's CAN network but I'm a little confused as there are two CAN interfaces in STM32F407 - CAN1 (Master, PB8 and PB9) and CAN2 (Slave, PB5 and PB6). Why do we need two interfaces? Can you...

usb host MSC send&receiveData

Posted on June 01, 2015 at 11:27 I made a project with stm32cude mx for stm32f401 discovery, discovery board is usb msc host, send a command to devide (usb msc device) then receive data form device my project connected and saw all infomati...

Khoa Tran by Associate II
  • 1258 Views
  • 1 replies
  • 0 kudos

Problem caused by NRST pin to perform system reset

Posted on June 15, 2015 at 10:26Hi,I am using STM32F405.The NRST pin is connected to Vdd through a 100k pull-up resistor and to GND with a 0.1uF capacitor, just follows the design of STM32F4-Discovery. The NRST pin is also connected to GND with a 2-...

How to specify external interrupt rather than event

Posted on June 15, 2015 at 10:41 Hi, Using the cube 4.8.0 I configured PA2 to be GPIO_EXTI2 because I want an interrupt generated when the signal connected to that pin goes low but the code that gets generated for me looks like this:   /*Configure G...

markb by Associate II
  • 1612 Views
  • 2 replies
  • 0 kudos

Compilation error with c++11 dialect

Posted on June 09, 2015 at 15:44Hi, I would like to use C++ 11 dialect with ac6 tools suite. But I get a compilation error that I'm not able to handle. Code : register char* stack_ptr asm(''sp''); Error : error: expected '=', ',', ';', 'asm' or '...

JulienD by Senior
  • 1525 Views
  • 5 replies
  • 0 kudos

READ from OTP

Posted on June 12, 2015 at 09:48Hejcan anyone tell me how to read from OTP. If possible put some sample code.Thank you ..

arunl4g by Associate II
  • 2278 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.