STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX & STM32F4 Discovery and a Simple HID USB issue

Posted on August 05, 2015 at 19:03I have build and tested the STM32cube Demonstration project using MDK-ARM for the STM32F4 Discovery and it worked fine.   So I tried my own very simple project using STM32Cube interface to create the source for a US...

jowen by Associate II
  • 908 Views
  • 1 replies
  • 0 kudos

Can Stm32 chips working at -55 degree? Is screening possible?

Posted on August 07, 2015 at 15:21We are trying to design a circuit which may need to work at -55 degree. And our current design is with stm32, which is very powerful.Here comes my questions:1. Does stm32f4 series have -55 degree (temperature) versi...

cyqdtc by Associate II
  • 1875 Views
  • 3 replies
  • 0 kudos

FATFS frustrating problem

Posted on August 07, 2015 at 16:40Hello again!I'm trying to read from sd card using SDIO. I've succesed to tun it on STM32f103 @72Mhz and after a while I managed to read at about 10Mb/s. But when I ported this files to STM32f407 it hangs somewhere i...

STM32f4 SPI Busy Flag

Posted on August 07, 2015 at 03:03 Hello all, I'm trying to communicate with a nokia 5110 LCD. The nokia 5110 has a slave select bit that I am setting using a GPIO pin (because I'm not entirely sure how the NSS bit for SPI works). My probl...

Problem with starting a debuging session

Posted on July 29, 2015 at 14:52Hello, I came across a problem which is about starting a debbuging seession on my System Workbench for stm32 (system Win7 x64). When I'm trying to debug my source code an information appears:Error in final launch sequ...

dooz by Associate II
  • 3055 Views
  • 6 replies
  • 0 kudos

STM32F3 timer3 ch1 interrupt

Posted on August 07, 2015 at 09:58Hello, I'm trying to set my timer3 on ch1 to make an interrupt with some frequency (100Hz). The idea is to switch it on and off by using a USER button situated on my stm32f3 board. I programmed it but it sometimes c...

dooz by Associate II
  • 1384 Views
  • 2 replies
  • 0 kudos

Can-Bus Error

Posted on May 12, 2014 at 19:56The original post was too long to process during our migration. Please click on the attachment to read the original post.

muhammet by Associate II
  • 15311 Views
  • 26 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.