2015-08-07 1:22 AM
Hi,
Is there any USB host example without class-specific driver? I see some examples in the Cube lib, but all are class-specific eg HID/MSC/etcI would like to have a 'direct' comms between a F7-disco and an external USB device via plain usb endpoints.So, I have to see how to communicate from a host application to the external device via usb pipes/endpoints.Is there something that I can have as an example project for that?RegardsChristosWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.