STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Generating single pulse on GPIO pin

Posted on July 12, 2012 at 11:25I want to generate single pulse with given length on GPIO pin on STM32F4 Discovery kit. I wanted to use timer in OnePulse mode. So I was planning to use TIM4 and TIM12, becouse I need 6 independent pins for pulses. Bu...

honza by Associate II
  • 7273 Views
  • 11 replies
  • 1 kudos

Srf02 on STM32F4-Discovery per I2C and show on Computer

Posted on August 13, 2015 at 15:46Guten Tag,ich habe nur einen SRF02, der ich mit einem STM32F4-discovery verbinden m�chte.Wie kann ich die gemessene entfernung auf Computer bekommen?K�nnen Sie mir vielleicht hefen bei einem programm code f�r CoIDE?...

wilsan01 by Associate
  • 1110 Views
  • 1 replies
  • 0 kudos

USART on STM32F4 discovey Board

Posted on August 11, 2015 at 12:30Hi all...,,I have an stm32f429zi based discovery board with me and newly woking on ST series. Actually I want to run USART/UART on my board to enable serial communication with other devices..but I am facing a troubl...

maharaj by Associate II
  • 1531 Views
  • 2 replies
  • 0 kudos

What is the minimum power CAN bus solution?

Posted on August 03, 2015 at 19:31We could use a 100 device CAN bus, but we have limited power for the system. Total power would be about 2-3 watts. How low power is possible. Total length of the bus is about 15m. Other requirements for the processo...

LMI2 by Lead
  • 4862 Views
  • 6 replies
  • 0 kudos

Create a fault on purpose

Posted on August 01, 2015 at 01:01I would like to test all my hard fault and friends (MemManage, BusFault, UsageFault, etc) fault handlers.  Essentially, I'd like to log their occurence to an I2C EEPROM.  I have all the HardFault handling working (a...

STM34f429i Discovery i2s/i2c question

Posted on August 13, 2015 at 08:52Hello everyone.I am building a simple car audio/video player, and the 429i with the LCD built into it seems perfect. I want to use a different DAC, specifically Ti's PCM5122, so that I can use higher grade amps, amo...

Communication STM32F3 to STM32F4

Posted on August 13, 2015 at 09:42Hi Friends,I'm working in a company temporarily. They gave me two boards. STM32F303VC and STM32F429ZI. I have one project to do. This project is about to communication between two boards. It's simple but i'm new in ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.