2015-08-13 6:43 PM
I am trying to use TIM4 in external counting mode, I have managed to configure it in external counting mode, but the count I am getting in watch 1 window is random. I am using ground pin of board to give input to PB7 and I expect it should give me one increment in the count when I remove it. but it is not so, can anyone tell me what wrong in my code. (Similar problem was posted in some other thread but could not find exact solution)
I want to get count of rising pulses from external signal:My Program is:
Main.c
/******************************************** */ /* Includes ------------------------------------------------------------------*/#include ''stm32f4_discovery.h''TIM_ICInitTypeDef TIM_ICInitStructure;uint32_t aa = 0;/* Private function prototypes -----------------------------------------------*/void TIM_Config(void);/* Private functions ---------------------------------------------------------*/int main(void){ /*!< At this stage the microcontroller clock setting is already configured, this is done through SystemInit() function which is called from startup file (startup_stm32f4xx.s) before to branch to application main. To reconfigure the default setting of SystemInit() function, refer to system_stm32f4xx.c file */ /* TIM Configuration */ TIM_Config(); while (1) { aa=TIM4->CNT; }}/** * @brief Configure the TIM4 Pins. * @param None * @retval None */void TIM_Config(void){GPIO_InitTypeDef GPIO_InitStructure;TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; /* TIM4 clock enable */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM4, ENABLE); /* GPIOB clock enable */ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE); /* TIM4 chennel2 configuration : PB.07 */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP ; GPIO_Init(GPIOB, &GPIO_InitStructure); /* Connect TIM pin to AF2 */ GPIO_PinAFConfig(GPIOB, GPIO_PinSource7, GPIO_AF_TIM4); TIM_TimeBaseStructure.TIM_Period = 65535; TIM_TimeBaseStructure.TIM_Prescaler = 0; TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM4, &TIM_TimeBaseStructure); TIM_TIxExternalClockConfig(TIM4, TIM_TIxExternalCLK1Source_TI2, TIM_ICPolarity_Rising, 0); TIM_Cmd(TIM4, ENABLE);}#ifdef USE_FULL_ASSERT/** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */void assert_failed(uint8_t* file, uint32_t line){ /* User can add his own implementation to report the file name and line number, ex: printf(''Wrong parameters value: file %s on line %d\r\n'', file, line) */ while (1) {}}#endif/** * @} */ /** * @} */ /******************* (C) COPYRIGHT 2011 STMicroelectronics *****END OF FILE****/2015-08-13 7:40 PM
I guess I'd troubleshoot this by using another timer to generate a 50 Hz signal, and then jumper that to PB7, and use a 1 Hz ticker to periodically print out the TIM4->CNT value.
The code doesn't look objectionable, and PB7 should be free.2015-08-14 12:06 AM
2015-08-16 7:01 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.