STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX freezes when generating code

Posted on August 11, 2015 at 10:26Hi,STMCubeMX is freezing every time I try to generate code for an STM32F429 project.  This is my first time using it, but everything so far has been pretty straightforward, and I haven't given it any crazy parameter...

njansen1 by Associate II
  • 3973 Views
  • 6 replies
  • 0 kudos

NOKIA LCD_6610 wrong STM32F107

Posted on August 21, 2015 at 16:24The original post was too long to process during our migration. Please click on the attachment to read the original post.

aubin by Associate II
  • 836 Views
  • 0 replies
  • 0 kudos

stm32f0 spi l3gd20

Posted on August 21, 2015 at 13:20The original post was too long to process during our migration. Please click on the attachment to read the original post.

SOLVED: STM32L151 MCO/PLL doesn't configure after reset

Posted on August 20, 2015 at 17:14I want to avoid using a 12MHz external crystal for another IC, so I set the MCO to the PLL, with the HSI feeding the PLL.  It works great when I flash the chip, but after a reset, it doesn't work.  Everything else i...

STM32F103RB and Totem Pole drive problem

Posted on August 20, 2015 at 12:06Hi I am trying to drive the output from pin PA8 (needed because I use it for TIM1 PWM) from 3.3V to 5V using an external totem pole drive circuit. Problem is no matter what I do the voltage of the output signal afte...

STM32CubeMX templates for Nucleo Boards

Posted on August 20, 2015 at 20:06Where can I find a template for the Nucleo boards; specifically the STM32F070RB-Nucleo and STM32F411RE-Nucleo offerings?   I am looking for the *.ioc file.

STM32 discovery board console Port driver

Posted on August 21, 2015 at 09:04Hello All,I started working/learning micripython using STM32F407 discovery board. The board I'm using is already with micropython (as my colleague used it earlier).I connected board to Windows PC and in ST Link util...

STM32L Discovery PWM

Posted on December 16, 2013 at 11:28 Hello, I tried to post this to the following thread, since this was my initial guidance to configure PWM, but was unsuccessful due to some permission error: https://my.st.com/public/STe2ecommu...

klemen by Associate II
  • 2077 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.