2015-08-11 1:26 AM
Hi,
STMCubeMX is freezing every time I try to generate code for an STM32F429 project. This is my first time using it, but everything so far has been pretty straightforward, and I haven't given it any crazy parameters that would seem unreasonable.The exact steps to reproduce the problem are: Load the IOC file (pasted below). Click Project -> Generate Code. It will display a progress bar, and will basically stay there forever (hours, etc). I've tried it several times, and it does the same thing every time.I will try re-generating the project and trying that, but figured I'd post this here to see if anyone else has had the problem, and to see if anyone here could re-create the problem. Here's my 'STMF429ZETx.ioc' file:http://pastebin.com/8hR9gveSAnd an image of the app, in its frozen state:http://imgur.com/pOawxylOh, my OS platform is Windows 8 on a pretty standard Lenovo laptop. My Java JRE version is 8.0.51.16.Any help would be appreciated.Thanks!2015-08-11 2:12 AM
Hi jansen.neil,
Which version of CubeMx are using? The last one is 4.9.0. Could you change your machine? -Shahrzad-2015-08-11 7:26 AM
Hi,
STM32CubeMX version is 4.9.0.I made a new project and tried to duplicate the settings section by section, and it actually worked (didn't freeze), although I'm not sure why. If I do a diff on the two *.ioc's they differ, but I can't figure out why one would work but the other one would make it crash. Either way, I guess it's working now.I'm still having a problem getting the project imported into either Rowley CrossWorks or ac6 SystemsWorkbench. I've not been able to get either of them to compile. Will spend a few more hours on it to make sure it's not anything stupid that I'm doing.. then I might be back for more help. This whole process has been extremely daunting but will hopefully worth it in the end.2015-08-12 10:48 PM
Now when I open up my new file, it still freezes up.
This is extremely frustrating and causing me to lose a lot of time. STM32CubeMX should not just lock up like this. It's clearly a bug or some unhanded corner case, but unfortunately there's not much else that I can do at this point.Can someone possibly reproduce this behavior on their machine? Is there any more information that I can provide to help track this down? Are there older versions that may be more stable? Is there anything else that I might be doing wrong?2015-08-13 1:37 AM
Hi jansen.neil,
Your .ioc file is needed in order to try to reproduce your issue. Could you please share it?-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2015-08-15 5:56 AM
Hi,
You will find a link to the .ioc file in my first post.2015-08-21 7:43 AM
Hi jansen.neil,
I generated a project with your .ioc file on SW4STM, I compiled it and I did not have any compilation error. Try to re-instal SW4STM and make right steps to setting the path of your project. Sorry to not be able to help you more. -Shahrzad-We’re moving the ST Community to a new platform to give you a better and more reliable community experience.