STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F407VG Clock presclalers

Posted on August 21, 2015 at 21:02Hello,I have couple of questions and doubts about STM32F407VG MCU setup I would like to clarify a bit.Q1: Do all the timers have the same clock source (system clock - PLL, HSI or HSE)? Because I have to divide APB1 ...

STM32F401Cx I2S MCLK

Posted on August 29, 2015 at 09:09Hi,I use STM32F401CE chip which has I2S peripheral but has no dedicated pin for MCLK.Is there a way for generating MCLK on a different pin ? Kind regards #i2s-mclk

ztraiger by Associate
  • 1260 Views
  • 1 replies
  • 0 kudos

STM32F7_Discovery not loading Demo images.

Posted on July 30, 2015 at 13:52Hello ST community, I have download latest version of STM32Cube for F7 mcu and I can easily compile the demonstration project using Keil. But the program seems to have no access to images (I figured out that this has...

pablo by Associate
  • 2203 Views
  • 4 replies
  • 0 kudos

ADC External Trigger

Posted on August 26, 2015 at 19:47 Hi Every One, My problem is I am not able to configure my ADC to start a conversion from external pulse, I want to use ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_RisingFalling; ...

puneethj by Associate II
  • 2947 Views
  • 6 replies
  • 0 kudos

STM32 Category 5 EEPROM write blocking.

Posted on August 06, 2015 at 23:29I've got an STM32L151RET6. This is a category 5 device. My understanding from the manual is that the on board EEPROM is in a separate bank (0x08080000) so that writes will not block reading from program flash. Howev...

edward2 by Associate
  • 882 Views
  • 1 replies
  • 0 kudos

stm32f215 - reading pulses

Posted on August 31, 2015 at 15:30I'm working with a microcontroller stm32f215. This device have a wheel of time (single encoder) connected to PF8 pin - TIM13_ch1. How best to accomplish reading this time round? Using the capture? Using the interrup...

william2 by Associate
  • 851 Views
  • 1 replies
  • 0 kudos

UART HAL driver usage

Posted on August 06, 2015 at 16:41HelloI am using NUCLEO L053R8 (STM32L0) , Keil uVision 5.15 and ST-Link (embedded in the nucleus board). I let CubeFx a FW program using CubeFx with HAL enabled.All compiles wellI can use the the blocking transmit f...

stanzanim by Associate III
  • 1284 Views
  • 1 replies
  • 0 kudos

STM32F4 Possible ADC Configuration?

Posted on August 05, 2015 at 19:29Hello all,I am using the ADC1 regular conversion or ADC1/2 dual-mode regular conversion to acquire a video signal.  The dual-mode is used at higher frame rate.  In both case, I am using the DMA. This part is working...

keaven by Associate II
  • 1072 Views
  • 1 replies
  • 0 kudos

SPI1 clk problem

Posted on August 06, 2015 at 15:20Hi. I'm using STM32F107VCT6 in a project. I need to remap the SPI1 signals to pins PB5 PA4/5/6. when i send the data from SPI1, i see the waves of MOSI but cannot see the wave of SCKL (PA5). why cannot see the waves...

aubin by Associate II
  • 1313 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.