STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Developing custom boot-loader for STM32F103

Posted on September 08, 2015 at 22:27I am developing a custom bootloader for the STM32F103.  The general plan is that there are two Micro-vision projects - one for the application (0x08040000) and one for the boot-loader (0x08000000).  In general th...

richm by Associate II
  • 1772 Views
  • 2 replies
  • 0 kudos

STM32F103 RS-485 only with HSI and HSI calibration?

Posted on September 08, 2015 at 09:21It isa goodidea to usetheSTM32F103communicating overRS485(38400bps)onlyHSI clock? STM32F103 will works in temperature -10 + 50C.I was looking atthe possibility ofuser calibrationHSI,toodo not understand. ST say. ...

asrock70 by Associate II
  • 2036 Views
  • 4 replies
  • 0 kudos

Bug in CMSIS_OS for FreeRTOS V1.02

Posted on July 29, 2015 at 17:09This file was provided in the L4 release V1.0.0.osSemaphoreWait should return an int representing how many tokens are remaining.  However, the implementation supplied instead returns a value of type osStatus.  They ar...

STM32F4 RTC interrupts

Posted on September 09, 2015 at 07:22Hello, I had a quick question is it possible to setup the RTC to trigger Alarm interrupt and Wakeup counter interrupt in the same program. This is needed because I use Standby for long sleep (~1s) and Stop mode f...

matas by Associate II
  • 870 Views
  • 1 replies
  • 0 kudos

High Level Timer/ADC/DMA Help

Posted on September 08, 2015 at 17:49I'm working on a sound-reactive project with the STM32F405 that samples ADC for FFT.  I'm currently using double-buffered DMA triggered by TIM3 TRGO.  Everything is working but it's very rough around the edges an...

craig by Associate II
  • 1762 Views
  • 3 replies
  • 0 kudos

Occasionally Missing Interrupts

Posted on September 07, 2015 at 13:44 I have an STM32 system that works correctly most of the time but occasionally fails to service interrupts. I wonder if there is something I am missing in my understanding of the NVIC: The system is built a...

Ultrasonic receiver

Posted on September 08, 2015 at 18:51  The original post was too long to process during our migration. Please click on the attachment to read the original post.

fiulala by Associate II
  • 1038 Views
  • 1 replies
  • 0 kudos

6 step motorcontrol

Posted on September 08, 2015 at 08:13The original post was too long to process during our migration. Please click on the attachment to read the original post.

binonso by Associate
  • 1116 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.