2015-09-08 12:21 AM
It is
a good
idea to use
the
STM32F103
communicating over
RS485
(
38400bps
)
only
HSI
clock? STM32F103 will works in temperature -10 + 50C.I was looking at
the possibility of
user calibration
HSI
,
too
do not understand
. ST say.High-speed internal oscillator of 8 MHz, typically). At 25 °C, the HSI has an accuracy of ±1% typically, this is factory trimed.
The accuracy value of the RC frequency increases to the maximum value of -2% - +2,5
%
over temperature. -10 +105C. It can say, typically error is less than 80kHz. Maximum error is -160kHz +200kHzWhy is it
then
user triming RCC_CR register step 40kHz and user trimming range +- 640kHz?2015-09-08 10:33 AM
Asynchronous serial does have some tolerance for mismatched baud rate clocks but you have to make some adjustments to allow for it. First, keep the baud rate as low as possible. The faster you go the worse the clock jitter will be. This shows up as framing or overrun errors caused by bits spilling over into the next frame.
Also, make sure there is a gap between characters so the UART has enough time to synchronize to the next start bit. Try setting both sides to two stop bits. This adds an extra bit time for the UART receiver to detect the next start bit. Remember the accuracy is at the base frequency. When you use the PLL to multiply the clock the inaccuracy gets multiplied as well. That 1% at 8MHZ is 8% at 64MHz. Jack Peacock2015-09-08 12:14 PM
When you use the PLL to multiply the clock the inaccuracy gets multiplied as well. That 1% at 8MHZ is 8% at 64MHz.
The error magnitude might be 8x bigger, but 1% of 64 is 8x bigger than 1% of 8, it doesn't make it 8%.2015-09-08 10:05 PM
Just the
basic
clock error
is
not
increased
by multiplying.
For example 8MHz with 1% error = 8080000Hz 8080000*8=64640000 this is 64MHz +1% error2015-09-09 5:16 AM
+/-1% at 8Mhz is 7.92MHz to 8.08MHz. an 8x multiplier yields a clock anywhere from 63.36 to 64.64MHz, +/- 640KHz or effectively 8x the frequency spread without the PLL. It's semantics but it is 8% of base frequency error.
UART timing based on 80KHz vs. 640KHz potential clock jitter is significant. It's enough that ST won't spec the PLL with HSI to clock at the same multiple as the HSE. Sure, some dramatic license in interpreting percentages but it illustrates the problem with unstable baud rates. Aside from all the comments, I have used RC oscillators with the PLL to generate baud rates (not on ST parts though, these were 8051s). It did work, but the controller had some assistance from an external 48MHz USB SOF clock to keep the RC and PLL stable. I wouldn't recommend it for ST parts except certain M0+ devices that also use an external RTC crystal to keep the RC stable, and even then there has to be some time for the PLL to sync to the external oscillator.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.