STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Driver problem in stm32f30x_tim.h

Posted on October 20, 2015 at 12:58 Hi The driver version I am using is * @version V1.0.1 * @date 23-October-2012 Is this an old version? If yes then where do I get a newer one? My problem is when I call some of the funct...

JustMe by Associate III
  • 1083 Views
  • 1 replies
  • 0 kudos

STM32F042 USB - what is ''Activate OE''?

Posted on October 20, 2015 at 13:40There is an ''Activate OE'' checkbox in STM32CubeMX is USB section of the tree which enables a ''USB_OE'' pin on PA4. I can't find any occurrence of USB_OE either in datasheet or reference manual. Can anybody tell ...

ISR and data from CCMRAM?

Posted on October 20, 2015 at 03:03Hi!On a F303K8 in SysTick i have two functions that i would like to run from CCMRAM because SRAM isunder heavy load from multiple DMA channel transactions, i use EmBitz tools. The functions fetch variablesand data ...

USBH_CtlSendData()

Posted on June 19, 2011 at 18:57Hi:I have problem with this function - it just doesn't work if you want to send some data (> 0 bytes). The setup packet is sent and ACK is received but when data packet is sent no response. See example below:         ...

iozho by Associate II
  • 2418 Views
  • 4 replies
  • 0 kudos

STM32F4 low power clock settings

Posted on October 16, 2015 at 10:57Hey, I need to decrese the STM32F401 consumpion to a minimum, the only problem is that I am using SDIO to interface a microSD card. Since the current consumption depends heavly on the clock is it possible to use HS...

matas by Associate II
  • 4497 Views
  • 12 replies
  • 0 kudos

Selcting the bootloader

Posted on October 19, 2015 at 11:07Hi,I am using STM32F405RGT6 in my project. I want to know which boot loader it has? How to select boot loader? can anyone help me please..thanks 

audio Codec AK4556

Posted on October 19, 2015 at 20:55Hi uguysI seemsto have a small problem, I'm trying to send and receive some audiodata to a external codec, the codec is an AK4556.I usethe cubeMx to initialize the I2S.When I look at the signals. Everything looks f...

0690X000006057CQAQ.png 0690X00000605GdQAI.png
spa23 by Associate III
  • 1313 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.