2015-10-20 4:40 AM
There is an ''Activate OE'' checkbox in STM32CubeMX is USB section of the tree which enables a ''USB_OE'' pin on PA4. I can't find any occurrence of USB_OE either in datasheet or reference manual. Can anybody tell me what is it?
Thanks.2015-10-20 5:03 AM
> I can't find any occurrence of USB_OE either in datasheet or reference manual.
Maybe because it's USB_NOE... So much about Cube's consistency with the manuals.
RM0091, Ch.30.4.1: The output enable control signal of the analog transceiver (active low) is provided externally on USB_NOE. It can be used to drive some activity LED or to provide information about the actual communication direction to some other circuitry. JW2015-10-20 5:11 AM
Thank you, Jan.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.