STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32U5A5QJI6Q - Which Pins to Use for Programming ?

Hi,I am working with the STM32U5A5QJI6Q microcontroller and need guidance on the programming pins. I plan to program it using [SWD/JTAG (choose one)] with an external programmer like ST-Link.Could someone confirm:Which pins are used for programming v...

Resolved! USB PHY internal vs external?

Hi,in CubeMX for the STM32F750V8T6, there is an option for External PHY or Internal PHY (see screenshot below).What is the point of using external PHY? It seems to just add cost and complexity. Is it perhaps considerably faster?Thank you  

Ricko_0-1734938360174.png
Ricko by Senior III
  • 3558 Views
  • 3 replies
  • 3 kudos

STM32H743 Dual mode ADC in 8 bit resolution

Hi Experts! Summary: Question: Anyone know if the dual 8bit ADC mode is broken on the STM32H743 or what I could be doing wrong?Details:I am trying to get 8 bit dual mode ADC working on the STM32H743. I see one post on here that seems to indicate some...

image.png image.png
JShro by Associate III
  • 1744 Views
  • 2 replies
  • 0 kudos

adc error handler

hiim using stm32g474vet6timer1 is trigger mode ,timer3 slavemode, both timer1 and 3 operate at 5khztimer1 will trigger timer3 and timer3 will trigger adc at every 5khz ,im using adc in multimode dma ,now the problem is when initally i start these con...

FSMC Connection

Hello teamI'm working on the LCD display parallel connection stm32f4 series.Please check the FSMC interface; I've included my schematic. 

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.