STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HSE ext. clock with PLL

Posted on December 08, 2015 at 10:44 Hello, im using a STM32f103 with a external digital clock of 10MHz. By the PLL it was set up to 30MHz with fit to our application. I used the std. perherals library to configure the clock. I a...

CubeMX 4.12

Posted on December 04, 2015 at 17:19When will CubeMX 4.12 be available?Thanks

Pwm master slave synchronization

Posted on December 04, 2015 at 19:07Hello, I'm working with STM32F4 and I'd like to stop PWM after N periods automatically like explained in this [DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommuni...

lrosadev by Associate II
  • 1882 Views
  • 2 replies
  • 0 kudos

reverse supply through output

Posted on December 08, 2015 at 23:19My STM32F030 is SPI slave to another external MCU.  External host may turn the VCC of my STM32  off.  When this happens SPI_CLK and MOSI pins are still at +3.3V, and these signals back-supply my MCU through output...

STM32F4 RS485 and RTS pin

Posted on December 08, 2015 at 12:11Hello there,I need to implement rs485 communication using STM32F407. I am using MAX487 chip which has a direction pin. I have searched the forums for a hardware solution to this, and found a topic which says that ...

0690X00000605K1QAI.png

CubeMX broke SDIO DMA in latest update

Posted on November 12, 2015 at 15:04In the current release of CubeMX V4.11.0 using the latest F4 libraries, V1.9.0, a bug has been introduced that makes the SDIO DMA channels useless.  In the previous library set, V1.8.0, when the DMA channels were ...

STM32 NUCLEO extension board with Ardunio Uno

Posted on November 10, 2015 at 21:05Hi ,I am trying to develope Ble HID keyboard using Ardunio Uno and STM32 X-NUCLEO-IDB05A1 extension board.I am very new to this... I have gone through the STM32 quick guide. I could not understand whether I need t...

venky999 by Associate II
  • 1282 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.