STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F405RGT6 part numbering mystery U V W

Posted on December 09, 2015 at 12:18Can someone please tell me what adding U or V or W to this part number means ? As Farnell and RS stock them I do not expect it to be programmed specials. The datasheet is of no help (that I can find). I'm hazardin...

alan23 by Associate II
  • 2505 Views
  • 4 replies
  • 0 kudos

STM32L100C Discovery clock after reset

Posted on December 09, 2015 at 16:22I've started to look for the answer for the following question after finding out the problem with UART. It did not work correctly, and I tried to change baud rate from 115200 to 57600. After that UART worked.I use...

kozlovdmn by Associate II
  • 1491 Views
  • 2 replies
  • 0 kudos

STM3240G-Eval LCD

Posted on November 24, 2015 at 09:06Hi , I have the STM3240G-Eval board and currently I'm working on a project which in it I'll need to display text in the LCD. I searched the internet for some tutorial or examples of how to do it using STM3240G-EV...

STM32F4 Voltage issue

Posted on December 02, 2015 at 19:05 Hello everybody, First sorry for my english (I'm French). I am a student and i work with my partner on a project of three-motorized drone. For the control of the motors, we use a stm32f429ZI discovery ...

flash readback protection

Posted on November 30, 2015 at 16:38HiI am trying to enable flash read protection (level 1) on STM32L151 chip.I use this code section, at the beggining of my program: FLASH_Status FLASHStatus = FLASH_COMPLETE;  /* Unlock the Flash Program Erase cont...

yarona by Associate II
  • 1645 Views
  • 2 replies
  • 0 kudos

P-Nucleo-IHM motor control

Posted on November 10, 2015 at 23:13HelloI just received via MOUSER  my EVAL pack P-Nucleo-IHM001(related to motor control  ..  6 steps or FOC algorithms)Is there anybody by ST (or any institution) having some experience ?BestLouis

NSS stays low after disabling SPI

Posted on December 09, 2015 at 16:00MCU: stm32f103rf SPI: SPI1 without remap, MSTR = 1 SPI1 NSS pin PA4 configured as AF push-pull PA4 remains low independent of SPI state (SPE, SSOE). When PA4 configured as GPIO it is working fine. When running the...

STM3240G-EVAL OV2640

Posted on December 09, 2015 at 15:36Hello! I have evaluation board STM3240G-EVAL with camera module OV2640 onboard. How I can setup camera to resolution 640x480 in RGB565 format?

vlad23 by Associate II
  • 657 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.