2015-11-10 12:05 PM
Hi ,
I am trying to develope Ble HID keyboard using Ardunio Uno and STM32 X-NUCLEO-IDB05A1 extension board.I am very new to this... I have gone through the STM32 quick guide. I could not understand whether I need to program Arduino Uno or STM32 X-NUCLEO-IDB05A1.Can anyone help on this.Please guide me some if there any example programs for HID keybaord.Kind Regards,Ven #stm32-nucleo2015-11-19 5:11 AM
Hi d.ven,
You didn't said which Nucleo board are you using. If it is the STM32L053R8-Nucleo, I suggest you use the HID example available in STM32CubeL0 package under STM32Cube_FW_L0_V1.3.0\Projects\STM32L053R8-Nucleo\Applications\USB_Device\HID_Standalone.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2015-11-19 5:45 AM
Ok, he didn't say he was using a Nucleo board, he's using the extension board as a SHIELD and attaching it to an Arduino Uno board, which states it is compatible with.
http://www.st.com/web/catalog/tools/FM146/CL2167/SC2006/PF262191
He's going to have to write his own software on the Arduino Uno to utilize the board. So he's either going to have to download and understand the documentation, and write his own, or find someone in the Arduino Community to do that for him.2015-12-08 2:37 PM
Hi Clive, Mayla,
Thank you for the response.Clivel you were right. I was trying to useX-NUCLEO-IDB05A1
with Ardunio Uno R3.
But looks like, If I understood correctlyX-NUCLEO-IDB05A1
doesn't supportArdunio Uno R3
asthe document says it supports the
Ardunio Uno R3 connectors(I think not the processor). There is a power supply difference. Needs clarification from Mayla on this.
So now I got
STM32L053R8-Nucleo
board and
X-NUCLEO-IDB05A1
.
I want create HID Bluetooth Keyboard application that can send ASCII chars to iphone notepad.
Please suggest me where to start and point me the examples and documentation.I will have a look at HID_Standalone example( is there any documentation for this example?)We’re moving the ST Community to a new platform to give you a better and more reliable community experience.