STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H7S78 DK switch HSE clock problem

I am trying LTDC color keying application. LTDC uses HSI as clock source. I want to make all system clock HSE. Then I will be able to use PLL3 with HSE. However, the processor example I am using uses an external ram with boot_xip. All clock settings ...

OKesk.1 by Associate
  • 734 Views
  • 0 replies
  • 0 kudos

Resolved! problem receiving multiple data with ethernet

Hello,I'm using an STM32 F4 board as a TCP Server and the hercule application on my PC as a TCP Client.I follow the online tutorial proposed by controllersTech for the configuration.This is what my program does: If I send the message "1" to the serve...

Dreamer3D by Associate III
  • 1787 Views
  • 2 replies
  • 1 kudos

STM32F030T8C6 PWM Not Setting new PWM Value.

Hi.I have the following code. However when I try and update the arb value with anything it just does not reflect on the pin.Currently it is running a stepper motor. The stepper motor moves one step every time the pulse goes high.With that in mind I a...

table by Associate II
  • 1143 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.