2024-04-20 1:55 PM - last edited on 2024-04-21 12:51 AM by STOne-32
Hi All
I'm new to STM32 and I'm exploring it a little bit. I think I've found an issue in the HAL
in configuration Line is referred to the external interrupt line to be connected.
it is configured in the BSP with (void)HAL_EXTI_GetHandle(&hpb_exti[Button], BUTTON_EXTI_LINE[Button]);
where static const uint32_t BUTTON_EXTI_LINE[BUTTONn] = {BUTTON_USER_EXTI_LINE}; and BUTTON_USER_EXTI_LINE is 0x2000;
the problem is in the usage of Line (in all the stm32c0xx_hal_exti.c file!)
linepos is almost always 0 since EXTI_PIN_MASK is 1 and this is wrong. Removing the & all seems to work properly.
Since it one of the first test that I'm doing with the ST IDE and HAL might be I'm doing something wrong :D
2024-04-22 8:13 AM
Hello @STDoom ,
First of all, welcome in the ST community.
Is it possible to send you code ? Because I tried to have an EXTI interrupt with the BUTTON_USER and I'm facing no issue and it is working fine.
Best regards,
Simon
2024-04-22 8:31 AM
Hi
I've just created the example for the demoboard NUCLEO- STM32C0.
If it might help later I'll copy here the project but I think was this one (https://wiki.st.com/stm32mcu/wiki/Getting_started_with_EXTI)
2024-04-22 10:07 AM
2024-04-23 7:46 AM
Hello @STDoom ,
I confirmed your issue and I have submitted an internal ticket addressing your request to the dev team.
Internal ticket number: 179773 (This is an internal tracking number and is not accessible or usable by customers).
Your workaround is working. Thanks for your contribution.
Best regards,
Simon
2024-05-27 2:43 AM
Hello @STDoom ,
To fix the issue in the bsp header file "stm32c0xx_nucleo.h" line 191 you need to replace this code:
#define BUTTON_USER_EXTI_LINE GPIO_PIN_13
by this code:
#define BUTTON_USER_EXTI_LINE EXTI_LINE_13
This will be implemented for the Cube FW revision.
Best regards,
Simon
2024-10-30 10:34 AM
In this same example, now when code is generated for Nucleo board C031C06, STM32CubeIDE generates this code in the file stm32c0xx_it.c:
HAL_EXTI_IRQHandler(&H_EXTI_13);but when try to compile, it says:
../Core/Src/stm32c0xx_it.c:151:24: error: 'H_EXTI_13' undeclared (first use in this function) 151 | HAL_EXTI_IRQHandler(&H_EXTI_13);Making it unusable. Is there a way to solve it?
2024-12-30 1:39 AM - edited 2024-12-30 4:07 AM
I too noticed the issue that H_EXTI_13 was not defined by STM32CubeMX, when using a NUCLEO-H723ZG, STM32CubeMX 6.13.0, STM32CubeIDE 1.17.0.
You could define it yourself in stm32h7xx_nucleo.h, past the point of the decalartion of enum BUTTON_USER, I would sugest line 170, something like:
#define H_EXTI_13 hpb_exti[BUTTON_USER]
Be aware when STM32CubeMX regenerates the code, it may kill it again.
Since you sometimes need to fix HAL bugs, or add enhancements (for example LAN8742), or support for greater capacity EMMC memories, where there aren't user sections, it's best to NOT let STM32CubeMX interfere with your project, once starting off. It's probably more safe to use a separate directory if you want to add stuff later, and add/compare that against your project. Meld could be very useful for that, for example.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.