STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

EXTI rising falling with pin monitoring - issue

Posted on December 15, 2015 at 10:05 I'm using STM32F4 Discovery. I configured a GPIO pin PB8 for external interupt for both rising and falling edges, so that I have to reset a flag when it is high->low or set when low->high which is done by rea...

Problem Failed firmware STM32F7Disco

Posted on December 15, 2015 at 10:34Hi. Board http://www.st.com/web/en/catalog/tools/FM116/SC959/SS1532/LN1848/PF261641?icmp=pf261641_pron_pr-massmarket_jun2015&sc=stm32f7discovery-pr On board I found this file: FAIL.TXT - ''The interface firmware F...

how to set RTE in uVision5

Posted on December 15, 2015 at 03:46Hi, in the uart_printf example project(using HAL drivers), I see the RTE(Run Time Environment) for the project has all the entries below not selected(empty) which seems weird to me. What do these empty entries mea...

0690X00000602akQAA.jpg
ckim by Associate II
  • 1156 Views
  • 0 replies
  • 0 kudos

F407VG And Its UOTGFS

Posted on December 13, 2015 at 01:59 Workalot is struggling with enumeration of an USB VCP application. While USBRST and ENUMDNE interrupts are being captured no other interupts are. Perhaps a kind observer may glance over the register settings ...

Workalot by Associate III
  • 1139 Views
  • 1 replies
  • 0 kudos

STM32CubeMX improvement suggestion

Posted on December 03, 2015 at 10:33Hi CubeMX team,Thanks for making this wonderful user friendly tool !!I would like to see an option to have main.c generated as main.cpp file.Thanks, Rob #cpp-c++-main.c-main.cpp-cubemx

schelven by Associate II
  • 932 Views
  • 2 replies
  • 0 kudos

mxCube import to Arm Gnu Eclipse

Posted on December 03, 2015 at 18:49Hello there,Arm gnu eclipse ( http://gnuarmeclipse.github.io ) is a plugin for eclipse similar to openSTM32. It has its advantages, for example that user can use way more debuggers than only ST-LINK. I was wonderi...

stm32f407 encoder using MX bug ?

Posted on December 14, 2015 at 21:23i have used stm32f407 and timer 2 in encoder mode (in 4X mode) , but after long hours of debugging , i have found the problem with the IC1 and IC2 polarity , selecting this option will cause the timer to no count ...

0690X00000605K5QAI.png
eeng by Associate
  • 590 Views
  • 0 replies
  • 0 kudos

ST - testing

Posted on December 14, 2015 at 10:31Testing discussion #text #test #text #text

sluiset by Associate
  • 1351 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.