STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Nucleo board consuming too much on external power supply

Posted on December 15, 2015 at 13:32Hi!, I've got a Nucleo board, it's a L152RE Rev C.I've tested the example PWR_STP_RTC available for these boards and the board successfully lowered it's consumption from 9.3 mA (in running mode) to 1.5 uA (in stop...

mbruder by Associate II
  • 1585 Views
  • 3 replies
  • 0 kudos

Why I'm switching from STM32 to PIC32

Posted on January 26, 2013 at 19:19An Open Letter to ST Micro I'm switching my development projects from the STM32 to Microchip's MIPS-based PIC32. I'm a hobbyist, so my concerns may be different than the pros' here - and the impact of my decision o...

STM Nucleo and SPI

Posted on December 15, 2015 at 10:56Hello and thanks in advance.I have now a STM32F091 Nucleo. I am interested in running SPI on it. However by looking at the page of the product I can not tell which pins are for SPI or if it supports SPI at all. Fo...

d_aliaga by Associate II
  • 1312 Views
  • 2 replies
  • 0 kudos

SPI write

Posted on December 15, 2015 at 14:35Hi I have seen that spi has 16 bit buffer but only we can send 8 bit. Would like to know why it is like that ?

arunl4g by Associate II
  • 820 Views
  • 1 replies
  • 0 kudos

UART reception problem when SysTick Interrupt is enabled

Posted on December 15, 2015 at 13:41 I'm using STM32F411RE-Nucleo board and generating a project with Cube MX for System Workbench. The problem is that,HAL_UART_Receivefunction doesn't receive input from the user, even though I don't change any U...

USART does not get interruption from time to time.

Posted on December 14, 2015 at 10:41Hi, We are using an ARM STM32L100RC. We receive in our firmware a message of just two characters through the USART 1. At 9600 kbps it works ok, at 19200 it fails sometimes, but at 38400 it fails one in ten times (...

rvarona by Associate II
  • 2102 Views
  • 4 replies
  • 0 kudos

Same calculation time in both 36MHz and 64MHz

Posted on December 15, 2015 at 14:55Hi everybodyI am trying to implement some mathmatic calculations in STM32F103.I use HSI and PLL to provide 64MHz and 36MHz clock, considering Flash Wait State and enabling Prefetch Buffer. I expect that the calcul...

serial port debug question

Posted on December 12, 2015 at 16:29Hello All, Moving from the Motorolla 9s12 to the stm32.  Just got a eval board and after recovering from Register shock I am just trying to get some blinky lights and serial comm (USART) going which is what I wou...

USB Host HID EventCallback

Posted on December 15, 2015 at 12:16Dear,In my STM32F429 application I use a mouse or a keyboard The USBH_HID_EventCallback is common to both It would fine to have a different callback registered in the HID_Handle by USBH_HID_InterfaceInit() like it...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.