STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F469I-Discovery Audion Application is not working?

Posted on December 17, 2015 at 09:06I am using IAR EMBEDDED WORKBENCH 7.50.1.10273 (Common Components 7.3.1.3987)Audio application (which is located in ...\STM32Cube_FW_F4_V1.10.0\Projects\STM32469I Discovery\Applications\Audio\Audio_playback_and_re...

Uart interrupt

Posted on December 19, 2015 at 19:15 Hello, I tried to get working the uart with interrupt. I can send and receive data by polling with the function HAL_UART_Receive. First how I can do to check if a byte is in the data_register, because whe...

How to set and reset ADC1 VBAT channel with Cube

Posted on December 22, 2015 at 15:01Hello to all, I can set the ADC1 Vbat Channel für a STM32F2xx with HAL_ADC_ConfigChannel(). But how can I reset the bit in order to save the battery from leakage current? I could not find a cube function similar...

andywild2 by Associate III
  • 680 Views
  • 0 replies
  • 0 kudos

STM32F030 PWM Frequency changing!

Posted on November 01, 2015 at 07:54Hi!Actually I'm new in STM32.I have a problem in creating pwm. while making pwm in 20KHz with timer1, the frequency suddenly changes during the run! it is programmed to be 20KHz but it jumps to 2 or 3KHz.i want to...

IAP for STM32F0

Posted on October 08, 2012 at 09:10Dear Friends,I read document AN4065 of ST. it told that use must configure 2 conditions for application code, I understand condition setting linker 0x08003000 for KEIL compiler.Does anyone help me explain condition...

toantq3 by Associate II
  • 3846 Views
  • 7 replies
  • 0 kudos

[solved]STM32F7 NOR memory with FMC

Posted on September 07, 2015 at 11:34Hello, I have some problems with FMC when I try to port my code from SMT32F407(with FSMC interface) to new project based on STM32F746(with FMC). The only changes I've made are timings(adapted to 216 MHz clock) an...

rmszal by Associate II
  • 7046 Views
  • 14 replies
  • 0 kudos

STM32F469I-Discovery Audio application is not working

Posted on December 17, 2015 at 09:10I am using IAR EMBEDDED WORKBENCH 7.50.1.10273 (Common Components 7.3.1.3987)Audio application (which is located in ...\STM32Cube_FW_F4_V1.10.0\Projects\STM32469I Discovery\Applications\Audio\Audio_playback_and_re...

Some doubts on CubeMX

Posted on December 19, 2015 at 12:58Hi,I am using Nucleo board and Keil 5. I am using cubemx to configure the nucleo (STM32F103Rxx). My doubts are1. if i configured USART then, do i need to configure the pins (for USART) manually in code?2. If i con...

SS.Sagar by Associate III
  • 1177 Views
  • 3 replies
  • 0 kudos

STM32 Timer Reset on Capture

Posted on December 21, 2015 at 23:36Hi,I'm using STM32 micros for a while. Now I'm migrating and old firmware from a LPC17 cpu to a STM32F1 and I don't know if I can replicate one functionality.I need to start a timer that will generate a single fix...

mscaff by Associate II
  • 1292 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.