2015-12-17 12:10 AM
I am using IAR EMBEDDED WORKBENCH 7.50.1.10273
(Common Components 7.3.1.3987)Audio application (which is located in ...\STM32Cube_FW_F4_V1.10.0\Projects\STM32469I Discovery\Applications\Audio\Audio_playback_and_record\EWARM) is not working.When i clean and rebuild the project i get the error message :''Fatal Error[Pe035]: #error directive: ''Reading built-in header-file. If you used upper case, try #include <stdarg.h>'' C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.3\arm\inc\c\stdarg.h 9 ''Can anyone help me please..2015-12-22 3:07 AM
Hi kucukgoz.mehmet,
With IAR 7.3, 7.4 and 7.5, we are not able to reproduce the error. Please, verify if you are using C99 as a C dialect (project->option->C++ compiler->language). Otherwise, may be you can send the project, so we can help more. -Shahrzad-We’re moving the ST Community to a new platform to give you a better and more reliable community experience.