STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Ethernet initialization

Posted on December 22, 2015 at 09:13Dear ST team,I run into some problem with Ethernet due to some initialization missing. In my system I use an external DRAM for the bss section and the internal ram for the data which use DMA. The bss is initialize...

STM32CubeMX Project fails to enable CRC clock

Posted on December 21, 2015 at 20:12I'm building a test program under STM32CubeMX 4.12.0 (with latest peripheral libraries as of 12/21/15) that uses the STM32F207's CRC peripheral, and I have discovered that the autogenerated code isn't enabling the...

Steve H by Associate III
  • 2372 Views
  • 1 replies
  • 0 kudos

STM32F303 Eval Board CAN Normal Mode

Posted on December 22, 2015 at 02:06Hello! Referring to the CAN Networking sample codes in Cube MX F3 package, I tried it out by connecting 2 STM32F303 Eval Boards. I used a female-female connector to connect the two boards. However, I am not able t...

Getting older version of CubeMX

Posted on December 15, 2015 at 18:12Hi all, is it possible to get older version of CubeMX to track new issues? It would be excelent if there would be posibilty to choose which version you want to use.

STM32F373: SDADC1+DMA2+TIM3

Posted on December 17, 2015 at 20:28  The original post was too long to process during our migration. Please click on the attachment to read the original post.

life758 by Associate II
  • 1459 Views
  • 3 replies
  • 0 kudos

Cortex-M0 ADC Latency STM32F030

Posted on December 21, 2015 at 17:46Clarification needed... When does the ADC EOC Flag get set? Before or after the ADC_DR write latency? ADC clock settings: Pclk/4 = 40MHz/4=10MHz(ADC_CLK 100nS). Write latency spec: 8.5 fpclk typ. (8.5 * 100ns = 8...

Timer clockdivision and prescaler?

Posted on December 21, 2015 at 21:21Hello, I see in my TIM_Handle_TypeDef variable that I can change the values of clockdivision and prescaler, but what is the difference between these two variables? Martin

How to Enable the Backup Voltage regulator with STM32 Cube?

Posted on December 21, 2015 at 11:19Hello to all, I am currently converting my Code from ST Periperal Lib to Cube which is a hell of a work because EVERYTHING has changed. The function names, the structures, the constants. I am using a STM32F2xx. I ...

andywild2 by Associate III
  • 1722 Views
  • 4 replies
  • 0 kudos

Custom board design

Posted on December 21, 2015 at 15:50Hi,I'm a software dveloper working in Germany. Our company is planning to develop a data logger product with temp,humidity,3-axis and light sensors also with a serial flash memory.I'm working on nucleo-L053R8 boar...

gandhi by Associate II
  • 1138 Views
  • 1 replies
  • 0 kudos

[SOLVED] STMStudio doesn't work after update to windows 10

Posted on December 17, 2015 at 09:18Hi, Before I update my windows 8.1 to 10, STMStudio worked. After update and installation java 64bit it doesn't start. I have tried reinstall STMStudio, uninstall and install java but it still doesn't work. Other ...

office by Associate
  • 1916 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.