STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

MxCube STM32 UART DMA transmit

Posted on December 28, 2015 at 00:05 I have this older example, it has a Buffer[] and it is supposed to transfer to DMA: /**************************************************************************************/ char Buffer[] = ''The quick brow...

How to rotate lower and upper half-word of a 32-bit variable

Posted on December 28, 2015 at 10:23Hi. I would like to rotate lower and upper half-word of a 32-bit variable as in next example: var = 0x12345678;  --> I would like to get 0x56781234; How could I do this as fast as possible (time is critical)? I sa...

matic by Associate III
  • 1737 Views
  • 2 replies
  • 0 kudos

STM32L100 signature + A version

Posted on December 29, 2014 at 19:10Hello I have two questions regarding STM32L100RB line. 1) How is it with STM32L100RB/STM32L100RB-A versions? Is it so, that only STM32L100RB-A is available and how are those distinguished? I have one of very first...

pa2 by Associate II
  • 2825 Views
  • 6 replies
  • 0 kudos

STM32f103 pwm for step motor

Posted on December 29, 2015 at 09:54Hi  everyone:     I'm using stm32f103 to control an IC name A3967. I can now produce pulse, but hope to control the stepper motor arbitrarily stopped. This means that the PWM can send the exact number of stop send...

STM32 CAN Normal Mode

Posted on December 23, 2015 at 10:57Hello! I am working on STM32 board and I am able to make it work by hitting transmit and receive handlers on CAN loopback mode but not normal mode. Are there any additional settings that have to be changed for CAN...

akshayamk by Associate II
  • 3015 Views
  • 8 replies
  • 0 kudos

Sleep Mode Current Consumption

Posted on December 29, 2015 at 21:40Hi, I'm using the STM32F427ZGT6 uC.  During VBAT operation mode, I'm not certain how much current the battery would need to source.  Can anyone give a idea?  Thanks, Brian #vbat #sleep

error in adding cpp library to c project in keil

Posted on December 27, 2014 at 15:05hi every oneim trying to develop a c project in keil ,know i need to add a cpp library file to project & it shows error,i think it is because project uses c compiler & it cant compile cpp libraries,but i dosent ha...

mhdizgah by Associate II
  • 2874 Views
  • 3 replies
  • 0 kudos

Minimal configuration to restart PWM

Posted on December 29, 2015 at 22:42I am using the timer output to drive a buzzer.  It runs okay as it is but I have to completely reinitialize the timer counter registers each time I want to make a sound.  Don't the configuration settings persist? ...

kenneth by Associate
  • 1526 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.