STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USART interrupt problem

Posted on December 30, 2015 at 12:18I'm using a stm32f10x micorcontroller (steval-mki121v1 evaluation board) and i want to enable an interrupt event when a data is receive through the USART. The problem is that the interrupt never occurs after the d...

mauro2 by Associate II
  • 1774 Views
  • 3 replies
  • 0 kudos

SWO Viewer STM32F401/411 Nucleo problem

Posted on December 26, 2014 at 17:47Hi to all,I have F401 and F411 Nucleo boards.Both boards have STLink version ''V2.J23.M7 STM32 Debug+Mass storage'' installed.However, SB15 is connected, so STLink and PB3 pin (SWO) are connected.If I open STLink ...

tm3341 by Associate II
  • 5150 Views
  • 14 replies
  • 0 kudos

STM32F429I-DISCO SDRAM + DCMI troubles

Posted on December 30, 2015 at 17:40Hello, I have ov7720 camera connected via DCMI to 429-disco board, it works, but when im trying to use SDRAM some issues occurs. DCMI and I2C (to configure camera) stop work after initialisation of ram (BSP_SDRAM_...

rokko by Associate II
  • 1073 Views
  • 1 replies
  • 0 kudos

STM32F4 DiSCOVERY's micro usb port doesn't work

Posted on December 29, 2014 at 18:18I have an STM32F4Discovery board (STM32F407VGT6) and about a half year I created a program which communicate via micro usb between the board and the computer. Now When I run again that program, (maybe newer atolli...

dankom15 by Associate
  • 2695 Views
  • 3 replies
  • 0 kudos

Cube Project with STemwin generates linker error L6406E

Posted on December 30, 2015 at 14:24Hi, I genetrate a new cube project of STM32F746 discovery and let Cube activate all peripheral. No RTOS, Keil V5, generate files. Then I add the STemwin files and library to the project and compile. Everything is ...

Osto by Senior
  • 1690 Views
  • 3 replies
  • 0 kudos

USB device disconnect and connect in STM32L0

Posted on December 29, 2014 at 17:02Hi I just begin in STM32L0. I using my board for dev an USB example base STM32L053R8. And I have a confused about USB connect and disconnect.  I run a test case based on STM32L053R8_NUCLEO_USB for test. And I don'...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.