STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

missing defines in

Posted on December 29, 2014 at 12:55Some &sharpdefines of SDRAM for  STM32Cube F4 v1.3.0   can be found only in Discovery and Examples subdirs, and are missing in  STM32Cube_FW_F4_V1.3.0\Drivers\STM32F4xx_HAL_Driver folder In next Cube version they ...

ADC DualMode Interl

Posted on December 29, 2015 at 15:51hello I wanna use ADC Dual Mode Interl with DMA1. I use following code but it doesn't work! where is the problem?! I cannot use DMA2. Iused DMA2 for other peripheral.... &sharpinclude <stm32f4xx_gpio.h> &sharpincl...

sanaz by Associate II
  • 1281 Views
  • 4 replies
  • 0 kudos

Using stm32f4 to build a lightsaber

Posted on December 29, 2015 at 19:55Has anyone tried to build one of those lightsaber toys using stm board? I had this idea and would like to hear your opinion. So working with button and led is pretty easy. So when I would press the button the prog...

theanswer by Associate II
  • 1218 Views
  • 1 replies
  • 0 kudos

USB CDC demo on STM32L0 Discovery Board?

Posted on December 29, 2014 at 20:16Hello, I am switching an application from RS232-based to USB-based between the host (either Linux or Windows) and a sensor module. I am currently using an STM23L053C8 processor to gather data from sensors and send...

jsvirzi by Associate II
  • 800 Views
  • 0 replies
  • 0 kudos

How can I write every second with USB MSC STM32f105

Posted on December 13, 2015 at 18:14Hi everyone,I wanna write my variable to USB every second but I can't.I think it can be in while loop f_mount(0, &fatfs);        if(f_open(&file, ''0:OLCUM.CSV'',FA_CREATE_ALWAYS | FA_WRITE) == FR_OK)    {        ...

Non-std character in CMSIS source code

Posted on December 28, 2015 at 19:05 The boiler-plate header section of the .h files in the STM32 section of CMSIS have a stray non-standard ISO character the messes up standard unix / linux system tools, eg. grep , sed , etc. This seems...

estie by Associate II
  • 1121 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.