STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HAL vs standard peripheral library

Posted on December 30, 2014 at 15:10I just got STM32F4 discovery board, and i was reading the manual about the sample application and I got confused with 2 driver libraries provided by STMWhat is the difference between HAL in (STM32Cube_FW_F4_V1.3.0...

hosweetim by Associate II
  • 2455 Views
  • 3 replies
  • 0 kudos

stm32f2xx USART RTS/CTS

Posted on June 28, 2013 at 07:52 May I know how can I configure my STM32F205 microcontroler for USART RTS/CTS??? I could not find any resource on the net, and my codes are below but it doesnt work: anyone can help me to configure t...

ho by Associate II
  • 4380 Views
  • 13 replies
  • 0 kudos

STM32F429-iDisco is very easy crash, why?

Posted on December 30, 2014 at 22:27STM32F429-iDisco is very easy crash, why? After installing it into our metal box, it crash very easily. At the beginning, we guess the electrostatic from other board cause that, then we add a think plastic to isol...

Linda by Associate II
  • 1176 Views
  • 1 replies
  • 0 kudos

How to measure clock frequency inside of MCU?

Posted on December 29, 2015 at 16:06Hi. I would like to measure different clock sources with TIM16 and MCO as it is described in reference manual for STM32F303 uC, which I am using. I configured TIM16 input capture from remap (in TIM16->OR register...

matic by Associate III
  • 7472 Views
  • 10 replies
  • 0 kudos

CMSIS DSP Library RFFT question

Posted on December 30, 2015 at 22:37I was wondering if it is ok to call arm_rfft_q15 to do an FFT in-place. Of course, I will make the input array 2x the the real FFT length and load the real data vector in the first half of the array. #cmsis-fft

ingle by Associate
  • 880 Views
  • 0 replies
  • 0 kudos

STM32F429 LTDC Pixel Format

Posted on December 29, 2014 at 14:03I have a 24 bit RGB LCD (RGB888) connected to STM32F429.As we know the Pixel Formats supported by STM32F4 are ARGB8888, RGB888, ARGB1555, RGB565 etc. Is the pixel format that we set in the LTDC configuration indic...

mahendrai by Associate II
  • 1702 Views
  • 2 replies
  • 0 kudos

STM32CubeMX ethernet PHY

Posted on June 11, 2015 at 18:49Hello, It appears as though the PHY driver generated by STM32CubeMX is just for TI's dp83848c? I'm going to modify the driver the LAN8710A PHY, but it would be nice if Cube supported choosing different PHYs (i.e. diff...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.