STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 - HSE OSC 16 MHz fails to start

Posted on December 31, 2014 at 17:20 Hi, I have a problem with proper main clock configuration in STM32F030K6T6. I've connected an external crystal 16 MHz with 2x15 pF caps, but the HSE is not starting. Variable HSEStatus remains 0, so the PL...

slatybor by Associate II
  • 2972 Views
  • 7 replies
  • 0 kudos

F407VET6 not entering code - left nRST floating by mistake

Posted on December 30, 2014 at 04:46I goofed, big time. I'm new to the STM32F and I didn't follow the STM32F4 discovery schematic. I built a board that I wanted to power up from flash, and while I remembered the BOOT0 setting (GND), I left nRST floa...

siegelj by Associate II
  • 3558 Views
  • 8 replies
  • 0 kudos

Timer PWM and Counter question

Posted on December 31, 2014 at 16:53I am using an STM32F407I want to generate exactly 400 pulses on PE5 or PE6 with a 50% duty cycle.I believe PE5 can be connected to TIM9 CH1, and PE6 can be connected to TIM9 CH2I have the PWM code running and I ha...

barry by Associate II
  • 1110 Views
  • 1 replies
  • 0 kudos

using the flash as an EEPROM of STM32F3

Posted on November 25, 2013 at 17:50Hi, This is a post that was posted before in a wrong thread, this post was : I would like to store my data in memory when the computing is done and used the data for the next use. I don't have the EEPROM memory o...

hilwan by Associate II
  • 4527 Views
  • 19 replies
  • 0 kudos

problem in calling timer interrupt routine

Posted on December 30, 2014 at 05:19I am using timer2 and I am trying to generate an interrupt from it, so according to vector table the TIM2 ID is 44 so i  am defining an interrupt routine as __interrupt(44) void TIM2_IRQHandler() so why is it not ...

Changing the font size

Posted on December 30, 2014 at 22:41I am working on my final year project and i have to change font of my display on LCD..Only available fonts in library are 4Font16x24Font12x12Font8x12Font8x8i thought of creating my own font files but could not und...

aatif by Associate II
  • 4938 Views
  • 8 replies
  • 0 kudos

problem with running RTC program in stm32f103ret6

Posted on December 28, 2015 at 23:44hi (at first excuse me for my English) I use standard peripheral  example for implement RTC at stm32f103ret6. but this example runs in microcontroller to this line and after that stops. what is the problem? and ho...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.