STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F429 Cannot set baud rate less then 9600

Posted on January 08, 2016 at 22:58 I have a target board that is based on theSTM324x9I_EVAL, I need to use 2 UARTS, I set up UART4 and USART1 both at 1200 BAUD, my clock is 180MHz with HSE of 25MHz. The strange thing I'm facing is that (...

I2C: where is data from HAL_I2C_Master_Receive_IT()?

Posted on January 08, 2016 at 23:50 Hi, I'm attempting to read an I2C device withHAL_I2C_Master_Receive_IT(). A logic analyzer shows the data coming across the I2C bus, but where does it go? This is a st32f405, IAR, and CubeMx generate...

Installing ST-LINK/V2 USB drivers.

Posted on January 08, 2016 at 22:57 Hi, I'm a newbie, and I have just started working with STM32 and the GNU tools available, and can anybody explain what is correct from the following quote on how to install which is on ( http://gnuarmec...

mbmail4 by Associate II
  • 18517 Views
  • 2 replies
  • 0 kudos

STM32F7 Unlock Process

Posted on January 08, 2016 at 18:58I have an F7 processor that I cannot get out of sleep.  I can communicate with it using the ST-Link tool, however I am unable to debug the part anymore.  The JLINK unlock tool does not support the F7 parts yet.  Ca...

jon2 by Associate II
  • 954 Views
  • 1 replies
  • 0 kudos

Nucleo + netmf

Posted on January 08, 2016 at 16:58Exists there an version of netmf usable for nucleo board as NUCLEO-F446RE ? #nucleo #netmf #f446re

rs.jahn9 by Associate
  • 1064 Views
  • 1 replies
  • 0 kudos

STM32f1xx SPI DMA reset

Posted on January 07, 2016 at 21:05Hello,I am having difficulty recovering from failed SPI transfers when using DMA. It appears that the DMA controller maintains the state of the failed transfer and tries to complete the operation when the next tran...

ADC channel usage

Posted on January 08, 2016 at 16:26Hi all, Is it possible to have some ADC channels in continuous mode and some others in independent mode for the same ADC1? If YES, can you please post sample code on how to configure the same? Thank you.

nps by Associate II
  • 948 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.