2016-01-07 12:05 PM
Hello,
I am having difficulty recovering from failed SPI transfers when using DMA. It appears that the DMA controller maintains the state of the failed transfer and tries to complete the operation when the next transaction is started. The only way I have found to fix this problem is to reset the processor! The new DMA configuration is ignored. I do not see a DMA channel reset in the user manual. Disable/Enable the SPI interface does not clear the problem.How do you recover from an interrupted SPI transfer when using DMA?TIA #dma #spi #stm32f12016-01-08 6:24 AM
Before making any change to DMA registers you have to disable the DMA channel, not the SPI channel (but you should stop SPI too). After a fault disable the DMA channel and reprogram the DMA registers before enabling the channel again.
2016-01-08 8:24 AM
DMA_DeInit() doesn't work?
How about resetting the peripheral on the AHB? RCC_AHBPeriphResetCmd(RCC_AHBPeriph_DMA1, ENABLE); RCC_AHBPeriphResetCmd(RCC_AHBPeriph_DMA1, DISABLE);Or disassociating the DMA Rx/Tx on the SPI while you set things upWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.